cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 Can Bus receive Error

ASSAAD.ASSAAD
Associate II
Posted on February 24, 2015 at 10:50

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
ASSAAD.ASSAAD
Associate II
Posted on February 25, 2015 at 13:43

Solved ; buadrate issue

naeen reddy
Associate II
Posted on October 03, 2017 at 08:46

iam also faceing same problem can u please help me out of it

Posted on October 03, 2017 at 12:11

So what settings are you using and what baud rate do you need? 

Stating your own issue and facts might be more helpful in diagnosing your problem? 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 03, 2017 at 16:33

I can run the demo code, which is set to a loop-back mode, but I cannot get normal mode to work.

I think message is not going out of the transmit mailbox. Status is going to pending all the time.

♯ include 'stm32f4xx.h'

♯ include <stdlib.h>

CAN_InitTypeDef CAN_InitStructure;

CAN_FilterInitTypeDef CAN_FilterInitStructure;

CanTxMsg TxMessage;

int mailboxstatus,k,uwCounter,intistatusview;

int TransmitMailbox;

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

void CAN1_Config(void);

void CAN2_Config(void);

void NVIC_Config(void);

RCC_ClocksTypeDef RCC_Clocks;

void Can1WriteData(uint16_t ID);

void Can2WriteData(uint16_t ID);

void INTTIM_Config(void);

int main(void)

{

//INTTIM_Config();

SystemInit();

RCC_GetClocksFreq(&RCC_Clocks);

CAN1_Config();

NVIC_Config();

// CAN_FIFORelease( CAN1,CAN_FIFO0 );

while(1)

{

if( CAN_MessagePending( CAN1,CAN_FIFO0))

{

}

for(int y=0;y<0xffffff;y++);

for(int y=0;y<0xffffff;y++);

Can1WriteData(0x123);

}

}

void CAN1_Config(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_CAN1);

GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_CAN1);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_Init(GPIOD, &GPIO_InitStructure);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);

CAN_DeInit(CAN1);

CAN_StructInit(&CAN_InitStructure);

CAN_InitStructure.CAN_TTCM = DISABLE;

CAN_InitStructure.CAN_ABOM = DISABLE;

CAN_InitStructure.CAN_AWUM = DISABLE;

CAN_InitStructure.CAN_NART = DISABLE;

CAN_InitStructure.CAN_RFLM = DISABLE;

CAN_InitStructure.CAN_TXFP = DISABLE;

CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;

CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;

CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;

CAN_InitStructure.CAN_BS1 = CAN_BS1_6tq;

CAN_InitStructure.CAN_BS2 = CAN_BS2_8tq;

CAN_InitStructure.CAN_Prescaler = 2;

CAN_Init(CAN1, &CAN_InitStructure);

/* CAN filter init */

CAN_FilterInitStructure.CAN_FilterNumber = 0;

CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;

CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit;

CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000;

CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;

CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0;

CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;

CAN_FilterInitStructure.CAN_FilterNumber = 0;

CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;

CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit;

CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000;

CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;

CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FIFO0;

CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;

CAN_FilterInit(&CAN_FilterInitStructure);

TxMessage.StdId = 0x123;

TxMessage.ExtId = 0x01;

TxMessage.RTR = CAN_RTR_DATA;

TxMessage.IDE = CAN_ID_STD;

TxMessage.DLC = 8;

}

void NVIC_Config(void)

{

NVIC_InitTypeDef NVIC_InitStructure;

NVIC_InitStructure.NVIC_IRQChannel = CAN1_RX0_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x1;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

}

void Can1WriteData(uint16_t ID)

{

CanTxMsg TxMessage;

unsigned int i;

TxMessage.StdId = ID;

TxMessage.ExtId = 0x00;

TxMessage.DLC = 8;

TxMessage.Data[0] = 0x02;

TxMessage.Data[1] = 0x11;

TxMessage.Data[2] = 0x11;

TxMessage.Data[3] = 0x11;

TxMessage.Data[4] = 0x11;

TxMessage.Data[5] = 0x11;

TxMessage.Data[6] = 0x11;

TxMessage.Data[7] = 0x11;

mailboxstatus = CAN_Transmit(CAN1,&TxMessage);

for(i=0;i<0x00ffff;i++);

while(( CAN_TransmitStatus( CAN1, mailboxstatus ))!=CAN_TxStatus_Ok);

k= CAN_TransmitStatus(CAN1, mailboxstatus);

}

void INTTIM_Config(void)

{

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

TIM_TimeBaseStructure.TIM_Period = 41999;

TIM_TimeBaseStructure.TIM_Prescaler =1;

TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1 ;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

TIM_Cmd(TIM2, ENABLE);

}

void assert_failed(uint8_t* file, uint32_t line)

{

while (1)

{

}

}
Posted on October 03, 2017 at 16:35

iam not getting what is the problem .please help me out of this

Posted on October 03, 2017 at 16:37

You would need a second node to communicate with.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on November 30, 2017 at 09:37

Hi ..Did your problem get resolved? I am facing the same issue..STM32F4xx connected to busmaster.  Transmit status is pending always..And also I see Error Code 2001 ( Bus Error - Bit Error ( Rx) )