STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with switch/case

Posted on April 03, 2018 at 15:22 Hi I got a problem with a switch in my MCU. I use custom board with STM32F030C8T6. This here is part of my program: void rozkaz3(void) { switch(bufor[3]){ case 0: HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4,...

Jakub B by Associate III
  • 14148 Views
  • 34 replies
  • 0 kudos

CAN BUS Stress Test

Posted on March 30, 2018 at 14:48 I'm testing one application with 3 differente device that send a message with random command ID and random data on CAN bus every random timeout: two devices with two STM32L433 nucleo and one with STM32F446 nucleo a...

STemWin + FreeRTOS.

Posted on April 06, 2018 at 15:05Hello,STeMwin version 540.FreeRTOS version 9.0.1.IAR EWARM 8.20.1STM32F746NG with 32MB of external RAM.I'm trying to use STemWin in a multi-task environment however I'm not getting very far.  I had actually been usin...

UART baudrate configuration CubeMx

Posted on April 06, 2018 at 10:21Hello,I use the Nucleo-L476RG to send and read data by the UART, so for that I used STM32CubeMx,the goal is to send data in a Maximum of baudrate which is 10Mb/s as shown on the picture below, but the code is excuted...

Resolved! STM32F767: wrong FLASH_OPTCR default value

Posted on February 27, 2017 at 17:11RM0410, rev.2 defines 0xF0FFAAFD as default value for FLASH_OPTCR. Table 3.7.8 has a value of 0xFFFFAAFD. This value does make more sense.Please correct, if not yet already done.

Microcontroller suggestion

Posted on April 06, 2018 at 10:19Hello,I am a Masters student in Embedded Systems at KTH working on a thesis to develop a blasting monitoring sensor and wanted to hear your suggestions on uCs.My intent is to measure ground vibrations with 3 geophone...