STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power On reset behavior of STM32L071KZU3

Posted on May 16, 2018 at 16:29             We are using STM32L071KZU3 MCU in our design and providing 1.8V to VDD,VDDIO2 and VDDA domains of MCU.         The on-board source voltage to MCU is exactly 1.78V(instead of 1.8V). During power-up, we coul...

STM32F103 bootloader recover

Posted on May 07, 2018 at 23:46Hello!MCU: STM32F103REwhen i reset Read Out Protection from my bootloader (from bootloder sub-programm from RAM) i have a erased internal flash. Set ROP to 1 -> 0. All ok! But.. how i can back data write to first 4k?? ...

STM32 Embedded Software

Posted on May 09, 2018 at 10:21 Hi ! I have 2 binary files for 2 different function, I'm wondering if there is a stm32 embedded software who can help me to choose which binary run, through the UART ? I want to select the application I run andchan...

SWSTM32 build errors

Posted on May 16, 2018 at 08:04Hi,I am exploring X-NUCLEO_IDB05A1 with STM32L476RG Nucleo, And while building the Profile_central project, I am getting build errors in console. Errors like:arm-none-eabi-gcc: error: ..\..\..\..\..\..\..\..\Middleware...

Alpha Mr by Associate II
  • 2773 Views
  • 5 replies
  • 0 kudos

Resolved! Many problems with STM32-MAT

Posted on June 23, 2017 at 00:43Hello,I am having more or less the same kind of problems than the one in this post <LINK NO LONGER ACTIVE> I am trying a very simple program: a read IO block directly connected to a IO Write block. I started with Matl...