STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SAI issue on STM32H743BIT MCU.,

Posted on May 23, 2018 at 08:48Hello.,.,I used STM32F765BIT MCU SAI interface in slave  mode to capture 4 channel audio inputs(TDM mode), I am using DMA (in Circular mode) to receive the audio data and it is working fine , But now I am upgrading to ...

MCU(STM32F042F4) and file question

Posted on May 23, 2018 at 07:20My MCU is STM32F042F4.So I must be used example in STM32F042K6-Nucled.If i want used example in STM32F072RB-Nucleo.Because there is no PWM example in STM32F042K6-Nucled.Q1.How can i used example in STM32F072RB-Nucleo t...

STM32F0-disco printf USART

Posted on May 23, 2018 at 06:50Hi, I'm working with the STM32F0 Discovery board.I have a problem to use printf function with the USART.I'm using the classical way to redirect printf function (redefine _io_putchar and added _write function).So printf...

What's the problem to IRQ signal when applying interrupt encoder and PWM output on BLDC with STEVAL extension board

Posted on May 23, 2018 at 05:10The problem describes more detail here:Before I turn on the voltage source to the motor inverter, the encoder signal and IRQ work normally by testing a PIN which would change level each time reaching the interrupt.When...

Resolved! Problem with writing flash memory on STM32L4

Posted on May 22, 2018 at 02:34Hi,    I am trying to write a flash memory location on an STM32L496 and I can't get it to work.  From reading the manual, I understand that each location can only be written once, and it must be erased before it can be...

RCC_CR_PLLRDY not set depending on code size?

Posted on April 27, 2018 at 15:43I'm running into an issue where the program will time out on while(READ_BIT(RCC->CR, RCC_CR_PLLRDY) == RESET)in stm32l4xx_hal_rcc.c:839 depending on how much code compiled in main.c.  The program will execute fine wi...

Lab Guy by Associate II
  • 1547 Views
  • 3 replies
  • 0 kudos

Watchdog timer RESET status.,

Posted on May 22, 2018 at 07:36Hello.,I am working STM32F7 series MCU, In this I am using watchdog timer with 1sec timing configuration . Now on reset how to know whether it is watchdog reset or power on reset. Because I want configure some table on...

LTDC Register Write Problem

Posted on May 22, 2018 at 14:30Hi everyone,I'm using Atollic True Studio 9.0.0 for my STM32F746G DISCO board project. No HAL Drivers, no CUBEMX, programming mcu manually. I have a debug problem. After i build and download the code, pressing the 'res...

N ORhan by Associate III
  • 670 Views
  • 2 replies
  • 0 kudos

Resolved! Files missing from FP-IND-PLCWIFI1 zip file

Posted on April 25, 2018 at 23:26I downloaded the FP-IND-PLCWIFI1 software.When I try to build the project 'STM32F401RE-Nucleo' there are a number of header files missingsuch as stm32_spwf_wifi.h, stm32Fxx_nucleo.h and relay.h to name a few.I am usi...