2018-02-19 4:12 PM
Does ST have a processor in a SOT23 package ? 5 or 6pin would be great.
what is the smallest processor physically available ?
Solved! Go to Solution.
2018-02-19 5:06 PM
5x5mm is relatively small
If that's too big there is a 4x4mm part, and a 2.097x2.493mm wafer scale part
2018-02-19 4:28 PM
QFN is pretty small.
NXP once sent me an ARM chip on a tiny package the size of a pencil head. forgot its package name.
2018-02-19 5:06 PM
5x5mm is relatively small
If that's too big there is a 4x4mm part, and a 2.097x2.493mm wafer scale part
2018-02-19 6:01 PM
Was it this one ?
LS1012A 9.6 x 9.6mm ? a little over powered and tooo big,
The PIC SOT23 is very under powered.
anything else ?
2018-02-19 6:11 PM
lpc11a02uk/04uk.
wlcsp20.