STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743: What is the purpose of pins FDCANn_TXFD/RXFD

Posted on March 01, 2018 at 14:39We are currently setting up a project using STM32H743 and need to implement CAN / CAN-FD. When activating FDCAN1 or 2 in Cube as Mode 'FD', two additional checkboxes can be activated: Enable_FDCAN_TXFD and Enable_FDC...

GS1 by Senior III
  • 2450 Views
  • 4 replies
  • 0 kudos

F030 UART framing error

Posted on May 31, 2018 at 09:29Hello,I am trying to receive data from https://learn.adafruit.com/adafruit-ultimate-gps?view=all, it should output 9600bd. MCU is STM32F030K6T6. Rx/Tx are crossed as they should be, connected to USART1 (PA2/PA3). I am ...

Real USART2 INT number

Posted on May 30, 2018 at 21:44 USART2 INT number # 26 instead of # I'm building a new project that involve FreRTOS and USART2, when enabling the interruption for the USART2, (Configuration-> USART2 configuration->NVIC Settings) the application s...

ilde by Associate
  • 2381 Views
  • 5 replies
  • 0 kudos

Question on SBBTLE-RF module and the ST's API

Posted on May 31, 2018 at 10:46Hello,I'm using the SPBTLE-RF module (shield) with a nucleo (STM32L476RG). I use the sampleAppTht project given by ST.The SPBTLE-RF module is used as a server.I've have a few questions:   -the function aci_gap_set_disc...

5v Tolerant Pin Behavior During Reset

Posted on May 31, 2018 at 10:43Hi,In our project we have to connect an output from our MCU (STM32H753) to an enable pin of an external components. The external component works with 5v IO voltage, so we've connected the GPIO through a 5v 100k pull-up...

Yan Rosh by Associate II
  • 792 Views
  • 0 replies
  • 0 kudos

Problem in using ADC1 Channel 1 in DMA mode

Posted on May 31, 2018 at 10:18   Hi everyone! Currently I'm working with multi channel adc on STM32F103. And I tried to read ADC on 5 channel including ch0,ch1,ch2,ch3 and ch6 by using DMA. However, I met a problem that I cannot read the ADC value ...

Ly Tai by Associate
  • 865 Views
  • 0 replies
  • 0 kudos

Flash loader demonstartor not detecting device

Posted on May 29, 2018 at 08:44Hi all, am getting error from flash load demonstrator v2.8 when connecting STM32nucleoF401RE and X NUCLEO WIFI IDWO1M1 , when upgrading UART firmware  'unrecognized device  .. please reset your device and try again' or...