STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051 adc interrupt problem. Multiple channels.

Posted on June 27, 2018 at 09:27STM32F051 ADC sample 5 channels with interrupt.I'm trying to sample 5 channels using an interrupt. (I'll get to DMA later:0))If I set the sample time to ('ADC_SAMPLETIME_41CYCLES_5') or longer then the code works as e...

Rob1 by Associate II
  • 1190 Views
  • 1 replies
  • 0 kudos

GPIOs or serial shift registers

Posted on June 27, 2018 at 07:33Hi,For an application we need a bulk of digital inputs(comes from sensors- about 30 inputs) and a bulk of digital outputs(go to relays- about 15 outputs). which solution would be better?1- using a high count digital i...

External power supply instead of USB

Posted on June 27, 2018 at 12:01I would like to power my STM32F446RE with an external source instead of using USB. Can I simply switch the position of JP5 such that it is connecting the E5V pin and the middle pin, and then provide the supply to the ...

Solution: longer SPI cables via ''DualSPI''

Posted on June 22, 2018 at 01:12I'd like to share an idea, actually a working solution for a common issue:''Why I cannot use a longer SPI cable?''''How can I make a SPI cable connection longer and keep still a high SPI speed/clock?''Issue:Potentiall...

0690X0000060LN8QAM.png 0690X0000060LD4QAM.png

Resolved! STM32F769 overheating problem

Posted on June 26, 2018 at 20:23Hello, I have a PCB with LCD, SD-Ram, QSPI, CAN bus, SD card and everything works fine. I use a STM32F769Bi (208pins LQFP). Now I think the temp of the STM32F7 is very high (80-85deg). Normally I work with Stm32f103 a...

Independent watchdog timer (STM32H743)

Posted on June 08, 2018 at 15:19Hello.,.,I am using IWDG in our application, It is configured for 1SEC timeout . In this I have a requirement to know the Watchdog RESET status, As per reference manual I have seen the register RCC_RSR (bit 26th) but ...

Resolved! Which pin is LSCO on STM32L4R5?

Posted on June 26, 2018 at 01:53Which pin has the LSCO function on STM32L4R5xx?I can't find it in the documentation.  I found MCO available on pin PA8, but can't find LSCO.

HAL_QSPI function

Posted on June 26, 2018 at 18:39Hi,Why there is no HAL_QSPI_TransmitReceive() function like HAL_SPI does?Thx