STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Most basic setup for SWD to work?

Hello, i need help with na stm32l031k6, I want to just start the processor and read it with an st-link v2, I have connected BOOT0 to GND(i haven't added a 10k resistor, but that shouldn't be the problem ), NRST with pull-up 1k to VDD, VDDA and VDD ar...

LubO_o by Associate
  • 2155 Views
  • 3 replies
  • 5 kudos

Resolved! stm32F429BI + LCD does not switch-on the display

I am starting some test with this modulehttps://it.aliexpress.com/item/1005002482177244.htmlwith 7” lcdI have found only one example that run but with TouchgfxI have got the same ioc from this example to generate a new code and insert the functions t...

Ciuffoly by Senior
  • 13001 Views
  • 46 replies
  • 1 kudos

Resolved! Periodic PC sample packets via DWT

I am trying to persuade an stm32F412 to provide Periodic PC sample packets.Reference manual RM0402 implies it is doable (Configure DWT as a PC sampler)The "Cortex-M4 Technical Reference Manual r0p0" says "You can configure the DWT to generate PC samp...

Scopi by Associate II
  • 1221 Views
  • 1 replies
  • 0 kudos

Resolved! Custom board with STM32f446rRE: JTAG TDI not successful

Hello everyone,I am developing a custom PCB and am having a problem while trying to flash the chip.Before delving further, I need to say that I have made a mistake with routing the JTAG traces to 10pin JTAG connector and may have burnt the chip. I tr...

jtag_circumvent.jpg sys.png pins.png 70nKA_0-1742223736249.png
70nKA by Associate II
  • 1152 Views
  • 2 replies
  • 0 kudos

STM32H743 realtime audio processing with DSP

Hi there,this is my first post here and also the first time that I mess around with STM32 processors.A few months ago I decided to start a new project for realtime audio processing with DSPand the STM32H7 series seemed to me a good candidate for what...

psychegr by Associate II
  • 8783 Views
  • 11 replies
  • 0 kudos