STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2S bits rotated

HiI am working on project that receive several I2S streams from MEMS microphones. I found that "audio level" from second microphones pair had higher level then from other. After some analysis and SD lines swapping i found that I2S data received by se...

i2s_SD-0xAAAAAAAA_CK.png i2s_SD-0xAAAAAAAA_WS-fall.png i2s_SD-0xAAAAAAAA_WS-rise.png i2s_WS-fall_CK.png
max_verem by Associate II
  • 2968 Views
  • 9 replies
  • 0 kudos

Resolved! STM32L452 LSE not starting

I have an STM32L452 rigged to use an external clock so we can keep the RTC running. Schematic attached.X2 is a clock from SiTime, programmed to be 32.768kHz. C36 is a supercap acting as battery backup. I used STMCube to generate the startup code to f...

LSE_schem.png
SLevi.1 by Senior
  • 8843 Views
  • 18 replies
  • 2 kudos

Resolved! LTDC not starting STM32H7S7Z8J6

Hi, Currently we have received our first prototype batch of board with the STM32H7S7Z8J6. There is external flash and ram on the board also, but first we want to try a simple test where we will just use the LTDC interface without touchgfx to make the...

leddel32 by Associate II
  • 2049 Views
  • 3 replies
  • 0 kudos

Resolved! extremely slow sdram read write performance

Hi,I am using STM32H563ZI to design a new product, there is a SDRAM(W9825G6KH-6) connected to the MCU with 16bit width bus. The SDCLK is 125MHz while the MCU running at 250MHz.  The read and write to SDRAM address space are both OK. But the read writ...

mpu_attributes.png mpu_regions.png fmc_sdram_config.png
jasonj2 by Associate II
  • 2419 Views
  • 5 replies
  • 0 kudos