STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 nucleo board programming problem

I have a STM32L476RG nucleo board.Recently when I tried to program it using keil I found some error messages and I was unable to program it.I found that LD3 LED is glowing .Initially when the board was programmable it was not glowing.I am attaching e...

0690X0000060OTCQA2.png 0690X0000060OT7QAM.png

Steps to have external SDRAM work properly!

I'm editing linker and startup files according to the example "FMC_SDRAM_DataMemory" but i con not access SDRAM. In example, it has only 2 regions as FLASH and RAM but we have 5 regions as FLASH, DTCMRAM, SRAM1, SRAM2 and MEMORY_B1. Also how can an i...

N ORhan by Associate III
  • 1166 Views
  • 2 replies
  • 0 kudos

On STM32F4 discovery board we got accurate 7000 adc sampes but unable to read 7000 adc samples using stm32f030r8 using SPI. Please provide your inputs.

Hi,We are using ADS1292 to get the ADC samples and we had successfully read the 7000 sample with the help of imx6 processor, STM32F4 controller.But now our project requirement changed and we have to use the STM32F030R8 controller with same ads1292 bo...

Bhushan by Associate II
  • 1443 Views
  • 2 replies
  • 0 kudos

Can't reset I2C in STM32F407 to release I2C lines

Posted on January 12, 2017 at 08:18I am using an STM32F407 on a customer board and have trouble with the I2C handling.I am using the latest HAL HAL_I2C_MasterTransmitIT and HAL_I2C_MasterReceiveIT to poll data from a sensor.The problem is that after...

Can i read BOOT0 pin state from program?

Hello.Can i read state of BOOT0 pin in STM32F030F4P6?My uC always turn on with BOOT0 GND, but i need to have dual purpose pin BOOT0 and have possibility to read only state of this pin.

tt.353 by Associate II
  • 2405 Views
  • 5 replies
  • 0 kudos

FMC Timing registers can not be written!

Im working to use external SDRAM for STM32F746DISCO board and configuring associated FMC register. When ia start to debug i see that all of SDTR (timing) register bits are valued as F. I can write to SDCR and SDCMR registers but can not write to timi...

N ORhan by Associate III
  • 715 Views
  • 2 replies
  • 0 kudos