User Activity

Dear Community,as I read from other posts e.g. here: https://community.st.com/s/question/0D50X00009XkhBISAZ/stm32f4-discovery-usb3300-ulpi-phyit is possible that the STM32f407 discovery board can be successfully connected via ULPI interface to a USB3...
Dear Community,I was trying to make composite USB2.0 device (FullSpeed) consisting of a UVC and HID component. Both the components I’ve tested before as a standalone device successfully. However after making a composite device accordingly to the HID-...
Posted on July 11, 2018 at 11:43The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on July 05, 2018 at 16:49Dear Community,I am trying to migrate some code of a STM32F4 series µC relying on the StandardPeripheralLib to STM32F7 “low layer� driver concept. Unfortunately the LL-Driver concept is not that identical to Stan...
Posted on July 03, 2018 at 13:48I’ve setup a DSP application including a F32 FFT that takes on STM32F407 about 5 ms and on a STM32F429 approximately  .5 ms. The clock settings are in both cases the highest possible values (STM32F407 -> 168 MHz and...