STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Custom USB HID Tutorial?

Posted on June 10, 2018 at 15:54Hello,i want to use an accelerometer as an joystick over USB. My problem is, that all Tutorials on Youtube are not in english. So i can´t understand the important explanations. Alle tutorials not on Youtube are almos...

R. K. by Associate
  • 1426 Views
  • 1 replies
  • 0 kudos

LL I2C Address Ack Detection

How can I detect (from a master device) when a slave Acknowledges its address on the I2C bus? I can see on my oscilloscope that the slave Acks its address, but I can't figure out how to detect that Ack from the I2C registers on the master. I'm using ...

0690X0000060OVXQA2.png
abotha by Associate III
  • 1270 Views
  • 1 replies
  • 0 kudos

HAL_I2C_Master_Transmit OR HAL_I2C_Mem_Write

Posted on November 20, 2017 at 16:23Dear all we have stm32f373xx chip.MAX7313 Chip for LEDs. The connection is via I2C interface.We need to ON an LED or group of them depending on some Interrupt.We need to read the value about the LED status stored ...

BLUENRG-1 ble gatt connection timeout

Hi!I am using bluenrg-1.i want to know about gatt connection timeout.i don't want to occur gatt timeout.but after 30 sec, aci_gatt_proc_timeout_event is called and process stopeed.can i adjust this time to no limit?BLE_RC example have no timeout, but...

SJaeW by Associate
  • 1015 Views
  • 1 replies
  • 0 kudos

Hardfault exception in STM32F070CB

Posted on July 06, 2018 at 11:24Hi,I am facing hardfault exception while running my application on STM32F070CB which is Cortex M0 based micro controller. The function of this MCU is to Communicate with another on board Cortex A5 based MPU via UART a...

Satish M by Associate
  • 1157 Views
  • 1 replies
  • 0 kudos

UART Overrun Error

Posted on February 11, 2018 at 13:19HelloI am using a stm32f103rct6 microcontroller and I want to transmit and receive large size packets of data simultaneously and continuously. For this goal, I used HAL driver and UART and DMA peripherals.When I r...