STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 stop mode

Posted on February 23, 2018 at 05:39Hi Has anyone been able to get the STM32F7 in to stop mode. I've been trying to get the current down on my board but to no avail. After sending the following commands listed below, I still see a current of ~5mA. I...

LoRa CMWX1ZZABZ Power consumption

Posted on June 20, 2018 at 14:30Hi there,I am developing a custom board (F103 and CMWX1ZZABZ LoRa module). I have that the lora module goes into stop mode alone but every time I have tried to measure power consumptionbut it is always 1.22 mA when mo...

P M by Associate III
  • 1223 Views
  • 1 replies
  • 0 kudos

Bluenrg1 RTC

Posted on December 08, 2017 at 08:33How to use the RTC in bluenrg1?I want to use the Bluenrg1 for a watch application that use ble, but the datasheet note that the RTC clock is disabled in sleep mode, that prevent it to be used as a RTC that use pow...

cgh21 by Associate II
  • 1209 Views
  • 1 replies
  • 0 kudos

STM32L4 USB OTG host driver for CDC-NCM

Posted on December 18, 2017 at 00:06I'd like to ask for some help with developing a driver for STM32L4 USB host connected with LTE module as a device, which enumerates as CDC-ACM and CDC-NCM device. I've used code generated from Cube and added the r...

krestan by Associate II
  • 2198 Views
  • 1 replies
  • 0 kudos

possibly problem with the Hal NAND driver?

we used a SDRAM (ISSI 42-45S16160G 256MBit 16M*16b) on Bank 1 and a 512MB NAND Flash (IS34_35ML04G081) connected to Bank 2 and 3 on an STM32F429BIT6. Sporadically we get an 0 bit on a flash page, but this is no problem of the NAND (ECC did not detect...

odin by Associate
  • 977 Views
  • 1 replies
  • 0 kudos

How to Main Flash memory programming

Posted on July 15, 2018 at 05:31Hi?From the  <PM0075  Programming manual>  ? P15?Mass Erase  as below code is successful ?Now?I  want to Main Flash memory programming  ,  but  I don't  how to do it  .  Anybody Know?.....Thanks!/*********************...

peng jun by Associate II
  • 1206 Views
  • 1 replies
  • 0 kudos

Can't make HAL_UART_Transmit_IT to send data

Posted on July 09, 2018 at 13:57Hello All!This is my code:Better see this https://github.com/RadoslavMarinov/transfer/blob/78eadef8c1a6482051c0c091bf3aaddbebfcaf69/main.c for better view!!/* * main.c * * Created on: 4.07.2018 �?³. * Author: Radoslav...