User Activity

Posted on May 03, 2018 at 14:00I'm working with stm32vldiscovery and I'm going to use max232 for USART. I'm using usart1 (pA9 and pA10 as TX and RX).The question is witch is the best way to make it wortk correctly and safetly specially with the RX p...
Posted on April 17, 2018 at 17:43which is best to power up    ''' STM32VLDISCOVERY '''   via 5V pins and a ground or 3,3V ???also which is best to for Digital Input for STM32VLDISCOVERY, using 5v or 3,3V ???In the data sheet I found that bouth of th...
Posted on January 25, 2018 at 02:00Hi I'm new with stm32, I bought an stm32f0discovery but I can't work with it I wanna get help or some tutorial please.