STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476 I2C problem

Hi All,I've been struggling with this for a while now. I have designed a new board based on the STM32L476 to replace an old design using a PIC. I cannot for the life of me get the I2C to work.I have used STMCubeMX to pinmux and configure / generate...

0690X000006BuyUQAS.png

Mark and Space parity on UART?

Posted on November 07, 2013 at 00:26Does anyone know if you can set Mark or Space parity on the STM32 USARTS?I only found that you can set Even or Odd parity so far. I need to configure an STM32 for hardware that uses Mark and Space parity bits so a...

byrned by Associate II
  • 5329 Views
  • 8 replies
  • 0 kudos

Problem with synchronization between STM32F7 Nucleo-F767ZI and OV5642 camera by Omnivision. How setting the external synchronization of the OV5642 and Nucleo-F767ZI?

I have an issue because the DCMI stay in a busy state and never acquire data from the DCMI. I have configured the camera for a VGA resolution and i want acquire that data through parallel interface using the DCMI and DMA of Nucleo board.Please, i hop...

STM32f303 discovery user USB not getting detected

Hello,I am using STM32F3 Discovery board. I want to send the data from stm to usb comport of PC. I have initialized USB drivers in cubemx. But still when i plug in the board in USER USB socket the computer is not detecting it. One more thing is, is t...

T6963

Posted on July 12, 2009 at 20:55T6963

jaroslaw2 by Associate II
  • 6604 Views
  • 14 replies
  • 0 kudos

24 bit SPI TransmitReceive oddity

Hi. I think I have an idea why this does what it does, but wanted to ask advice anyway.I am interfacing an STM32F767 over SPI with an SSD2828 parallel RGB to MIPI bridge.It (amongst other options), uses what they describe as 24 bit SPI.I am using the...