STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C between 2 stm

Hi.I want to communicate between two stm32 of different cores via I2C, lets say between F0 and F7.F0 would be slave and F7 master.The idea is when user button on F7 board is pressed ,the control will shift to F0..but i don't know how to give a slave ...

asim khan by Associate III
  • 708 Views
  • 0 replies
  • 0 kudos

SMT32F1 I2c SCL stretching

Hi, allI have a project using a STM32F103c8t6 that works perfectly with HAL 1.4.0, but when I update a HAL to 1.6.1 version, the i2c device which is configured as a slave, after some writing or reads from the HOST it keeps the SCL in LOW, causing acc...

CBair by Associate
  • 656 Views
  • 0 replies
  • 0 kudos

pinout for stm32f429

hello I'm looking for a pinout for board stm32f429, a pinout that shows how the LCD tft (ili9341) is set to which pin on the board.

Code Generation from MC Workbench

Hi,I am interfacing a new motor to STEVAL-SPIN3201 board. It is a BLDC with four poles. In order to integrate the new motor settings, I am generating .h files from MC workbench 5.2.0. But here is the catch. The files generated by MC workbench does no...

ABasa by Associate
  • 747 Views
  • 1 replies
  • 0 kudos