User Activity

While Editing USER_LABEL on GPIO Configuration window facing the following issueneed to set common word for particular GPIO likePC0 ----> USER1_KEYPC1 ----> USER2_KEYPC3 ----> USER3_KEYPC4 ----> USER4_KEYnow i'm selecting all the GPIO in group select...
When Creating STM32Cube Project ,While Selecting Code Generation Option as "Add necessary library files as reference in the toolchain project configuration file"Then giving Finish will result the following"Code Generation could not be done because th...
I'm generating code using STM32CubeMX F4 1.24 with STM32CubeMX 5.1.0 for the boardNUCLEO-F446RE for IAR EWARM 7 versionThis application is simple LED blinking test for the new F4 cubeMX 1.24After generating code and compiling in IAR EWARM i'm gettin...
I'm using STM32CubeMX 5.0.1 for creating projectsWhile configuring GPIO using configuration window the properties windows on the bottom of selected GPIO pin overrides the visibility of other GPIO pins at the bottom on configuration window It is not s...
I'm using NUCLEO-446ZE Host to access USB KeyboardMy cubeMx version STM32Cube FW_F4 V1.21.0I configured all clock and 48Mhz for USB via PLLSAIPMain core run on 180MhzWhile connecting Keyboard I'm able to detectWhile accessing k_pinfo = USBH_HID_GetKe...
Kudos from