STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

the adc result in dual mode are not in the right order

hello i am using stm32f103 for reading a 10 adc channels and i am using Dual mode regular simultaneous with DMA , the result are loaded in a buffer.the problem is the loaded data from the ADC1 are in the right order (1st data is from 1st channel)bu...

H.Darwish by Associate II
  • 8939 Views
  • 10 replies
  • 0 kudos

UART set up in STM32L0

I want to stablish a UART communication between two boards (B-L072Z-LRWAN1 and 8PYA00-SIMCOM-EVB_V1.02). I tried to make a version of UART communication looking at all the examples provided by ST: static USART_HandleTypeDef huart; huart.Instanc...

pbdiazam by Associate II
  • 2569 Views
  • 5 replies
  • 0 kudos

no interrupts in low power (STM32L151)

Posted on January 18, 2018 at 09:50Hello everyone,I'm trying to make a device where the MCU (STM32L151) has to wake up periodically every 5 minutes and send a LoRa message. As such i want to put the device in a low power mode between messages. I rea...

IIC Slave causing issue

Hi I am using a STM32L433 IIC port as a slave. I am connecting it to another processor which has been used without any issues on another project so I know the connecting processor works fine as IIC master.I simply have set the processor up to simply...

SPI (Basics): Why do I get a signal at MISO (PB_4) when performing a write without any connection to this pin? I am using STM32F413 Discovery Board with mbed

Hi everyone, I am trying to connect my STM32F413 Discovery Board to a MAX30003 ECG but without any success. So I checked the SPI signals with a scope and discovered that I measure a signal on the MISO line as soon as I use a write command. All pins (...

jjens by Associate II
  • 3903 Views
  • 7 replies
  • 0 kudos