LIS2DW12 INT1?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-06-09 7:51 AM
Posted on June 09, 2018 at 16:51
Hi,
i am working on stm32l071, interfacing with LIS1DW12 i have configured
1. Write 64h in CTRL1 // Turn on the accelerometer // ODR = 200 Hz, High-Performance
2. Write 04h in CTRL6 // FS 2 g LOW_NOISE enabled
3. Write 20h in CTRL7 // Do not use low-pass filter for 6D, enable interrupts
4. Write 40h in TAP_THS_X // Set 6D threshold (6D_THS[1:0] = 10b = 60 degrees)
5. Write 80h in CTRL4_INT1_PAD_CTRL // 6D interrupt driven to INT1 pin
6. write 10h in CTRL3
getting satus SIXED register change the direction of 6D
but didn't get interrupt in MCU from INT1 LIS2DW12
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0