cancel
Showing results for 
Search instead for 
Did you mean: 

stm32l496g_discovery_sd.c hypothesis denied

Posted on June 08, 2018 at 13:19

Bugs in current, and older code trees

STM32Cube_FW_L4_V1.12.0\Drivers\BSP\STM32L496G-Discovery\stm32l496g_discovery_sd.c

...

/**

  * @brief  Initializes the SD MSP.

  * @note   The SDMMC clock configuration done within this function assumes that

  *         the PLLSAI1 input clock runs at 8 MHz.

  * @param hsd: SD handle

  * @param Params: Additional parameters

  * @retval None

  */

__weak void BSP_SD_MspInit(SD_HandleTypeDef *hsd, void *Params)

{

  GPIO_InitTypeDef gpioinitstruct = {0};

  RCC_PeriphCLKInitTypeDef  RCC_PeriphClkInit;

  /* Prevent unused argument(s) compilation warning */

  UNUSED(Params);

  HAL_RCCEx_GetPeriphCLKConfig(&RCC_PeriphClkInit);

  /* Configure the SDMMC1 clock source. The clock is derived from the PLLSAI1 */

  /* Hypothesis is that PLLSAI1 VCO input is 8Mhz */

  RCC_PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SDMMC1;

  RCC_PeriphClkInit.PLLSAI1.PLLSAI1N = 24;

  RCC_PeriphClkInit.PLLSAI1.PLLSAI1Q = 4;

  RCC_PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_48M2CLK;

  RCC_PeriphClkInit.Sdmmc1ClockSelection = RCC_SDMMC1CLKSOURCE_PLLSAI1;

  if (HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphClkInit) != HAL_OK)

  {

    while (1) {}

  }

...

The PLL share a common divided clock source via PLLM, in the critical example code for this platform the source is almost always the MSI in Range 6, ie 4 MHz and not an 8 MHz HSE

Resulting in the microSD card being super slow in the primary demo code, 24 MHz at the peripheral, 12 MHz on the wire, instead of twice that.

STM32Cube_FW_L4_V1.12.0\Projects\32L496GDISCOVERY\Applications\FatFs\FatFs_uSD_Standalone\Src\main.c

...

/**

  * @brief  System Clock Configuration

  *         The system Clock is configured as follows :

  *            System Clock source            = PLL (MSI)

  *            SYSCLK(Hz)                     = 80000000

  *            HCLK(Hz)                       = 80000000

  *            AHB Prescaler                  = 1

  *            APB1 Prescaler                 = 1

  *            APB2 Prescaler                 = 1

  *            MSI Frequency(Hz)              = 4000000

  *            PLL_M                          = 1

  *            PLL_N                          = 40

  *            PLL_R                          = 2

  *            PLL_P                          = 7

  *            PLL_Q                          = 4

  *            Flash Latency(WS)              = 4

  * @param  None

  * @retval None

  */

void SystemClock_Config(void)

{

  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  RCC_OscInitTypeDef RCC_OscInitStruct = {0};

  /* MSI is enabled after System reset, activate PLL with MSI as source */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;

  RCC_OscInitStruct.MSIState = RCC_MSI_ON;

  RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;

  RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;

  RCC_OscInitStruct.PLL.PLLM = 1;

  RCC_OscInitStruct.PLL.PLLN = 40;

  RCC_OscInitStruct.PLL.PLLR = 2;

  RCC_OscInitStruct.PLL.PLLP = 7;

  RCC_OscInitStruct.PLL.PLLQ = 4;

  if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    /* Initialization Error */

    while(1);

  }

...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee
Posted on June 08, 2018 at 16:44

Hello

Turvey.Clive.002

You are right, weconfirm the point in FatFs applications, it is OK for the Demonstrationapplication code main.c where in SystemClock_Config() it is indicated:

RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_7; /*!< MSI = 8 MHz. Do not modify this value used as SAI Source, MMC */

Our development team is aware about this issu, andstudying this point for fix in the coming release of STM32CubeL4.

Thanks and Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on June 08, 2018 at 17:07

The solution I had was to make the PLLSAI1 settings consistent with all the other L4 examples, as I recall several of the L4 NUCLEO's don't connect HSE to the ST-LINK by default.

/* Hypothesis is that PLLSAI1 VCO input is 4MHz MSI */

  RCC_PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SDMMC1;

  RCC_PeriphClkInit.PLLSAI1.PLLSAI1N = 48; // [7..87] whilst keeping VCO in 64 to 344 MHz range

  RCC_PeriphClkInit.PLLSAI1.PLLSAI1Q = 4;

The more hardened approach would be you compute this stuff on the fly so it was adaptive, or to try and keep the clock setting code in a centralized location

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 08, 2018 at 17:24

Clocking the SDMMC peripheral at 96 MHz yielded 25 MBps reads on a 16GB SAMSUNG eMMC chip

Currently talking to some individuals out of the European WDC/SanDisk office about eMMC support with

Przenioslo.Lukasz

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..