STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 HAL I2C Driver - Wrong Slave Address

Hi, I have a board with STM32F501R8T6 and AT24C02 & DS1307 RTC are connected to I2C2. Earlier i had used custom I2C driver and interfaced them with a 8051 controller without any issues. Now since there is a need to change the I/0 pins config in ARM ...

PR.19 by Associate II
  • 1805 Views
  • 2 replies
  • 0 kudos

Ethernet driver in STM32Cube did not implement PTP interface

I'm a developer of the open source system zephyr, I need to implement PTP in Ethernet, but I found that stm32f4xx_hal_eth of STM32Cube did not implement PTP interface. Why not add this part of implementation,I request to implement the PTP interface i...

Jxudong by Associate
  • 1786 Views
  • 4 replies
  • 1 kudos

STM32F042: External clock and clock output

As described before (https://community.st.com/s/question/0D50X00009sWdDqSAK/stm32f042-bootloader-activation) I want to use 2 STM32F042 as CAN controller. So far I planned to use the internal HSI RC oscillator, but a +-5% tolerance seems critical for ...

0690X000006CHJZQA4.png 0690X000006CHJeQAO.png
harald by Associate III
  • 2109 Views
  • 3 replies
  • 0 kudos

HMAC digest doesn't match expected (STM3221G-EVAL)

I just purchased the STM3221G-EVAL board and I am working through some examples. I am currently using running the HMAC example and it runs fine. However I am unable to get the HMAC to match the test vectors provided in the specification (https://tool...

OOmen by Associate II
  • 1571 Views
  • 5 replies
  • 0 kudos

Problems with PWR_MODE STOP and the wake up with Timer LPTIM1

The LPTIM1 interrupt is running. But if I use the EnterStopMode function, the controller is not gone at the stop mode (LED1 come directly). If I use the EnterStopMode function the second time, the controller goes into the STOP mode and after few sec...

AxelMC by Associate II
  • 1990 Views
  • 6 replies
  • 0 kudos