STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 timer is too slow

Hi,I'm using STM32H755 Nucleo board and I'm trying to use TIM2 to trigger Dual ADC conversion. M7 core is running FREERTOS and M4 is bare metal. ADC is controlled by M4 core. DMA is used to transfer data to M7 and then M7 is using ethernet to transfe...

clock.PNG TIM2.PNG
mosamasa by Associate II
  • 2009 Views
  • 6 replies
  • 0 kudos

Resolved! STM32G0B1CCT6 FDCAN Bootloader

Hello, According to reference manual/datasheet/ANs, it exists some documents that are pointing out that FDCAN2 is the capable bootloader port for upgrade.In ANs and reference manual, it is specified that FDCAN bootloader mode is available on PD0 & PD...

RomainP by Associate
  • 1276 Views
  • 3 replies
  • 3 kudos

Bootloader on STM32H730 with FreeRTOS

Hi everyone,I’m currently facing an issue related to bootloaders and FreeRTOS on STM32 microcontrollers, specifically the STM32H735 and STM32H730.Here’s the background:STM32H735 Development Board: I have successfully implemented a bootloader that jum...

HispaEmo by Associate III
  • 1421 Views
  • 1 replies
  • 0 kudos

MULTI_Q U545REQ

I used MultiQ example 'LPBAM_DMA_MultiQExec' I change code for U545REQ board but it doesn't work.i found some issueThis is 'LPBAM_DMA_MultiQExec' codetatic void MX_LPDMA1_Init(void) { /* USER CODE BEGIN LPDMA1_Init 0 */ /* USER CODE END LPDMA1_...

dlagyals by Associate II
  • 1288 Views
  • 2 replies
  • 0 kudos