STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Buffer size error when compiling the embedded webserver on STM32F7 with a different display image than provided. Any ideas?

I am running the embedded web server on the STM32F7 and I changed the linked image that is displayed on the MCU. It compiles, but doesn't display. After investigating, a buffer size error is being thrown and consequently the main code gets stuck in...

TSnyd by Associate
  • 746 Views
  • 0 replies
  • 0 kudos

Access ETM only with code without the use of debug kits

My board is Nucleo F401RE. This is the first time I've ever been doing this.I am using a pointer to the main registry of ETM, its address I read it on the datasheet.My problem is that wanting to change the bits of this log I do not change it the corr...

LRusc by Associate
  • 619 Views
  • 0 replies
  • 0 kudos

Vdda Vs Vdd Stm32l433cc

HiMy stm32l433cc circuit has two different LDO, one for Vdd and another for Vdda. Can you tell me please can i run my controller without Vdda power? I need to turn on/off analog power when i need it. Is it possible on stm32l433cc?

mkozi.17 by Associate II
  • 2883 Views
  • 5 replies
  • 0 kudos

Resolved! Incorrect SPI clock frequency

Hello,I'm trying to get data from an external ADC (18bits) with an STM32l476RG nucleo board. There is a lot of overhead and I will improve it later but even the frequency clock is not fast enough. I don't understand why but the maximum clock frequenc...

Sirac by Associate III
  • 4298 Views
  • 7 replies
  • 0 kudos

Read data from ADC and send it via I2S

Hi guys! In my project Im reading samples with the adc at 48Khz using timer interrupts and adcConvCallbacks, load them in a buffer of 256 samples and when the buffer is full I send it via i2s to the DAC . Im using two buffers, when the bufferA is ful...

MDoro by Associate II
  • 1770 Views
  • 3 replies
  • 0 kudos

STM32L152 ADC- Can not read from address 0x1FF800F8U

Hi,With helping of CubeMX I measure voltage on battery (ADC channel 0) using ADC in DMA mode. I also measure internal refference because my VDDA is not know in advance.Once these 2 values are measured I need to convert the RAW data to mVolts.I use da...

JAN R by Associate III
  • 1937 Views
  • 6 replies
  • 0 kudos

USART Rx & Tx communication code

Hello,I am a beginner to Nucleo-64 board programming and I am trying to work on USART communication of it. I am using NUCLEO-L476RG board and STM32CubeLL library for configuring USART and starting communication with it. Programming Scenario:I have co...

VDesa by Associate II
  • 6164 Views
  • 13 replies
  • 0 kudos