Timer in STM32L071 works correctly in Debug mode but incorrectly in Run mode
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-07-09 11:23 PM
Posted on July 10, 2018 at 08:23
Hello,
I designed a board using STM32L071KZU6. I am using HAL_TIM_Base. The timer works correctly in Debug mode. But when I use run mode without debug, the timer takes longer. (I set 5s but it is 1-2 min). What problem with it? Please review attached file with my configuration timer and clock.
Thanks,
#debug #stm32_timers
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0