STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i cannot use X-CUBE-MEMS1

https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-mems1.htmli downloaded this software.i also used the gui program. but i have to read under 0.01g so gui...

khyun.8 by Associate
  • 780 Views
  • 0 replies
  • 0 kudos

software reset problem if reset from a task

Posted on January 21, 2014 at 14:29I use NVIC_SystemReset() in order to reset the system.  I am using STM32F103 in my application and RTX rtos. The problem is that if  called NVIC_SystemReset() before the RTOS started, the software reset worked. If ...

huiyan by Associate
  • 3911 Views
  • 5 replies
  • 1 kudos

How to calibrate the RTC accuracy?

I'm using the STM32F767ZI MCU and with its RTC function. But my quartz crystal is not accurate. According to the document of the MCU, the accuracy can be calibrated (it said in page 35/255: Digital calibration circuit with 0.95 ppm resolution, to com...

HFeng.2 by Associate
  • 811 Views
  • 0 replies
  • 1 kudos

How to check the SPL version?

I found a version macro in the library but it seems to be wrong. Please see attachment. What should I do to check the SPL version in the code?

TMark.8 by Associate II
  • 1141 Views
  • 0 replies
  • 0 kudos

MB1314B AMOLED board schematic

Hello, We are developing a watch-like wearable device with LCD. STM32L4R-Discovery board is a nice reference design for STM32L4R+AMOLED development. It would be also nice to have a schematic for the adapter board MB1314B, which the AMOLED is attached...

Resolved! Trim clock from pulse-per-second GPS signal?

Using STM32F030 / F042. I have a GPS receiver onboard which produces a very accurate pulse-per-second signal (~40ns). I want to use this timing source to keep the system clock, or at least the RTC accurate. The user may wander in and out of GPS recep...

AKrup by Associate II
  • 3747 Views
  • 6 replies
  • 0 kudos

Resolved! CAN filtering

How does one define the filter for a CAN A message, when the ID is only 11 bits?If using 16-bit filter, what should be put to the EXTID[17:15]?

Question about mixing HAL and LL library for UART

Hi,I try to use both HAL and LL library for UART. When I config UART with cubeMX for LL library, I found all functions with HAL library in my code doesn't work. when I say it doesn't work, I mean the code passed compiling but doesn't do anything. Th...

jeffz by Associate II
  • 913 Views
  • 0 replies
  • 0 kudos

ETH on NUCLEO STM32H743 is not working

Hi,My Question is related to the PHY LAN8742 mounted on that board. GPIO Configuration for this part is OK, but obvioulsly the 25Mhc clock generator is not working, and i guess this is the reasonfor no response from the PHY. I expect a 25Mhc signal...