what is the reason I2C peripheral does not work in master transmit mode in this program ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-07-24 5:07 AM
i did not use standard peripheral library or cubemx to write this program . and i did it programming registers.
as you know when data in TXDR register is sent the TXE flag in ISR register become one .
i have checked ISR while no data is writen in TXDR and TXE=1 ( i have done this by debugger ).
after that i write data in TXDR , TXE becomes '0' but never becomes '1' , means that data will not send.
i have used counter. the code is inserted below .
i do not know if this helps you answering me but one of the reserved bits of the register ISR becomes '1' by hardware after i write data into TXDR , i don't know if this shows an error .
I hope you can help me .
#include "stm32f0xx.h"
uint8_t acc[7],data[2],contr1;
uint16_t acc_x,acc_y,acc_z;
uint32_t status,cr2;
void i2c1_conf (void);
void i2c_write( uint8_t nby , uint8_t *data ,uint8_t addr);
void i2c_read( uint8_t nby , uint8_t *data, uint8_t addr);
void delay_ms(uint16_t delay_m);
//void I2C1_IRQHandler (void);;
int main()
{
i2c1_conf();
data[0]=0;
i2c_write( 1 , data,0x6c);
//I2C1->CR2 |= I2C_CR2_START;
//status=I2C1->ISR;
while(1)
{
i2c_read( 6,acc,0x3b);
acc_x = (acc[1] + acc[0]<<8);
acc_y = (acc[3] + acc[2]<<8);
acc_z = (acc[5] + acc[4]<<8);
}
//return 0;
}
void i2c1_conf (void)
{
RCC->AHBENR |=RCC_AHBENR_GPIOAEN;
GPIOA->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR9|GPIO_OSPEEDR_OSPEEDR10;
GPIOA->PUPDR |= GPIO_PUPDR_PUPDR9_0|GPIO_PUPDR_PUPDR10_0;//A9=>SCL A10=>SDA
GPIOA->AFR[1] |= (4<<((9-8)*4)|4<<((10-8)*4));
RCC->CFGR3 |= (1<<4);// I2C1SW SYSCLK
RCC->APB1ENR |= RCC_APB1ENR_I2C1EN;
I2C1->CR1 &= ~ I2C_CR1_PE;
I2C1->TIMINGR =0x50330309;//400KHZ ANALOG FILTER ON //or 0X00801CAB OR 0x00C31845 OR 0x00C31C45(BEST I THINK) or 0x00C01A4B;
I2C1->CR1 &= ~( I2C_CR1_ANFOFF|I2C_CR1_DFN );//ANALOG FILTER ENABLE DIGITAL fILTER OFF
delay_ms(10);
I2C1->CR1 |= I2C_CR1_PE;//|I2C_CR1_TXIE ;
I2C1->CR2 &= ~(I2C_CR2_ADD10|I2C_CR2_RELOAD|I2C_CR2_AUTOEND);
I2C1->CR2 |= 0X69<<1;
// NVIC_EnableIRQ(I2C1_IRQn );
}
void i2c_write( uint8_t nby , uint8_t *data ,uint8_t addr)
{
I2C1->CR2 &= ~I2C_CR2_RD_WRN; //WRITE MODE
I2C1->CR2 |= (nby<<16);
I2C1->CR2 |= I2C_CR2_START;
status = I2C1->ISR;
//while( ((I2C1->CR2 & I2C_CR2_START)==I2C_CR2_START));
while (!((I2C1->ISR & I2C_ISR_TXE) == I2C_ISR_TXE));//can be removed
I2C1->TXDR = addr;
//I2C1->CR2 |= I2C_CR2_START;
for(uint8_t contr =0; contr<nby ;contr++)
{
while (!((I2C1->ISR & I2C_ISR_TXIS) == I2C_ISR_TXIS))
{
status=I2C1->ISR;
contr1=contr;
}
status=I2C1->ISR;
cr2=I2C1->CR2;
I2C1->TXDR = data[contr];
}
while ( !((I2C1->ISR & I2C_ISR_TC)==I2C_ISR_TC));
I2C1->CR2 |= I2C_CR2_STOP;
}
void i2c_read( uint8_t nby , uint8_t *data, uint8_t addr)
{
I2C1->CR2 &= ~I2C_CR2_RD_WRN; //WRITE MODE
I2C1->CR2 |= (1<<16);
I2C1->CR2 |= I2C_CR2_START;
while (!((I2C2->ISR & I2C_ISR_TXE) == I2C_ISR_TXE));
I2C1->TXDR = addr;
while ( !((I2C1->ISR & I2C_ISR_TC)==I2C_ISR_TC));
I2C1->CR2 |= I2C_CR2_RD_WRN;//READ MODE
for(uint8_t contr =0; contr<nby ;contr++)
{
while (!((I2C2->ISR & I2C_ISR_RXNE) == I2C_ISR_RXNE));
data[contr] =I2C1->RXDR;
}
while ( !((I2C1->ISR & I2C_ISR_TC)==I2C_ISR_TC));
I2C1->CR2 |= I2C_CR2_STOP;
}
void delay_ms(uint16_t delay_m)
{
RCC->APB1ENR |= RCC_APB1ENR_TIM14EN;
TIM14->CR1 &= ~(TIM_CR1_CEN|TIM_CR1_UDIS);
TIM14->PSC =48000;
TIM14->CNT=0;
TIM14->DIER &= ~ TIM_DIER_UIE;
TIM14->ARR=delay_m;
TIM14->CR1 |= TIM_CR1_CEN;
while(!(TIM_SR_UIF & TIM14->SR));
TIM14->SR &= ~TIM_SR_UIF;
TIM14->CR1 &= ~TIM_CR1_CEN;
}
/*
void I2C1_IRQHandler (void)
{
if ((I2C2->ISR & I2C_ISR_RXNE) == I2C_ISR_RXNE)
{
data_r = I2C2->RXDR;
}
}
*/
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0