Posted on July 09, 2014 at 05:57Can any body have idea how to enable vertical scrolling in ILI9320 based TFT.Regads #lmgtfy #vertical-scrolling-ili9320 #rtfm
Posted on June 25, 2014 at 12:46Sir,I have successfully initialized USB port on Hi mini STM32F1V board now I would like to design a software routine to disable the initialized USB port plz help me out how to implement this.Regards #stm32f1-usb-p...
Posted on May 09, 2014 at 06:55PLZ HELP ME OUT HOW TO ENABLE LONG FILE NAME FORMAT WHEN USING FATFS LIB FOR 4 GB SD CARD #lfn #fatfs #fatffs-long-file-name
Posted on July 15, 2014 at 06:58Sir,Plz elaborate ''Alternatively just memcpy() your frame buffer to accommodate a new line at the bottom''I have set the values of vertical scroll registers as Register 61h = 0x0003(set VLE and REV bit to 1)Registe...
Posted on July 10, 2014 at 06:56I did not get what do you mean by embedded with the board?I am using HY-Mini Stm32V Borad and TFT is shipped with the board.This board using STM32f103 controlloer to drive the TFT.Regards
Posted on May 16, 2014 at 06:11 Hi What changes will be required in GUI_Text function to display converted data from Emwin font converter.
________________
Attachments : GLCD_Lib.rar : https://st--c.eu10.content.force.com/sfc/dist/vers...
Posted on May 13, 2014 at 07:54 I have used ''LCDvision'' to convert the fonts but when I used the converted data unknown symbols , lines or dots are appeared on TFT. Is there need to change the write to LCD function every time for every new f...
Posted on May 06, 2014 at 07:53 I have used the LCD_BMPmono function of that file only. I have used your proposed ''LCD_DrawPicture'' function of GLCD.c this function is displaying same Image multiple times on the screen. I got an ''Imag...