STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDMMC & SDIO - why max 1 SD card only?

I'm writing an SDMMC driver for my C++ RTOS - http://distortos.org/ - and there is one thing which really puzzles me, making it hard to decide about class hierarchy. In the Reference Manual for STM32F7 (but the same is true for other chips, both for ...

I2C pcb and pull-up

Good morning, I wanted to ask a question about the I2C interface.In particular on the routing of the pcb, I have a micro STM32 that is the master for i2c bus, then there are 2 slaves on the board and a connector to allow the connect of a third.The qu...

Complementary PWM at active low.

I have generated complementary PWM signal on STM32L496ZGtx. I used TIM1CH1 and TIM1CH1N. I am using one pulse mode so that every 1 second, I generate complementary signal. However one channel starts at active HIGH and another starts at active LOW. Ho...

RTC Time updated on reset

Hi,I'm running RTC on LSI Clock and transmitting data via UART2 but the RTC is not displaying updated values but while on reset it is showing updated values as shown in below image.Thanks & Regards,Vijay Rakesh.// Gobal Variable's RTC_HandleTypeDef ...

0690X000006DFmvQAG.jpg

Resolved! STM32F100C8T6 can't generate sinewave of correct frequency

The chip I am using is STM32F100C8T6.  I want to generate a sine wave with 40Khz between 0 to 2V ,but I cant't get correct frequency. I have finished reading STM32F100 datasheet (RM0041) and AN3126,AN4566. After that,I am writing a program based on t...

0690X000006DFk6QAG.png 0690X000006DFkBQAW.jpg
cTomm by Associate II
  • 1994 Views
  • 3 replies
  • 0 kudos

how to declare byte in STM32

I am using in adruino declarationuint16_t x;...byte lowerByte = lowByte(x); byte upperByte = highByte(x);Wire.beginTransmission(0x23); //Slave Address Wire.write(lowerByte); Wire.write(upperByte); Wire.endTransmission();to send bigger numbers over I2...

MNapi by Senior III
  • 2709 Views
  • 2 replies
  • 0 kudos

Resolved! The audio player demonstration

Dear In Application note AN3126 noticed that : “The audio player demonstration described in this section is a part of the STM32100B-EVAL demonstration firmware, which can be downloaded, together with the associated user manual (UM0891), from the STMi...

Bug in STM32L1 SDK (LL) samples

Projects\STM32L152RE-Nucleo\Examples_LL\USART\USART_Communication_TxRx_DMA\Src\stm32l1xx_it.cDMA handlers clear wrong flag (GI instead of TC):void DMA1_Channel6_IRQHandler(void){ if(LL_DMA_IsActiveFlag_TC6(DMA1)) {   LL_DMA_ClearFlag_GI6(DMA1);Versio...