STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI shift registers

Hello, In STM32F446RE mcu the block diagram shows 2 shift registers , but in STM32F407x spi block diagram it shows only shift diagram . which one is correct ? are these SPI IPs are different on these devices ? please clarify . i have attached the ima...

0690X000006DMsqQAG.png
n.serina by Associate III
  • 909 Views
  • 4 replies
  • 0 kudos

Hardware connection for uSD 4 Wire Bus

Hello,There is any schematic example for the connection between uSD and the STM32H7?I'm currently using a OLIMEX E407 with a STM32H7 instead of a STM32F4. It seems that I have problems with the signals integrity. I can read and write with a 1MHz cloc...

STM32H750 KEIL

I USED KEIL WITH STM32F750VB AFTER COMPILE AND RUN I UNDRESTAND NO HAVE ANY SPACE ADD FOR STACK FIRST VARIABLE ADDRESS IS FIRST MEMORY ADDRESS IF USED PUSH OR PUP CHANGE SOME FIRST VARIABE IN MEMORY HOW CAN RESOLVED THIS PROBLEM

How to Choose the Most Flexible NUCLEO 'Range'?

We've been using a NUCLEO-L433RC-P to prototype a low -power PCB and it has served us very well.We're now embarking on a new project where we're actually going to use the NUCLEO and create a PCB with a header to plug the NUCLEO into. I thought this ...

MBrow.13 by Associate II
  • 994 Views
  • 0 replies
  • 0 kudos

False LPTIM CMPM Interrupts ( STM32L071)

If the LPTIM CNT is close to the ARR value (0xFFFF) and i set the CMPM value, i receive the interrupt immediately (~1ms) instead of the time i set it. Because the LPTIM runs on 32kHz this happens every 2seconds for 4-5 interrupts.I dont seems to find...

DKilg by Associate II
  • 912 Views
  • 0 replies
  • 0 kudos

Using MSC to send data to GPIO PINS?

Can someone use MSC to send data to SPI or other GPIO Interfaces?I implemented a Project with Cube and now i want to test it by sending data through MSC to any GPIO or LED

arduo by Senior
  • 777 Views
  • 0 replies
  • 0 kudos

Resolved! Bug in MCU STM32L4 when trying to program the flash

I just run across a bug when trying to program the flash.You have to write two 32bit values for programming the flash. But if the first value is 0xFFFFFFFF it does not matter what the second value is. In the end there will always be written 0xFFFFFFF...

No I2C Clock signal after Restart Condition

Hello,I raised this problem in another topic I posted, but it is with another title and I'm not sure I will get there the help (title might be missleading).I have the problem after sending Slave Address and Register Address and creating a start condi...

0690X000006DUzQQAW.png
uli stone by Associate II
  • 5419 Views
  • 12 replies
  • 0 kudos

CAN on STM32F072C8

Dear ST sirs: We are using STM32F072C8, and we now have problem on its CAN bus. Like the below thread issue in the forum. However we did not see any reply on it.https://community.st.com/s/question/0D50X0000A4nF6FSQU/stm32f072c8-canbus-loopback-worki...

CHsu.14 by Associate II
  • 2440 Views
  • 3 replies
  • 0 kudos

Resolved! Time Triggered CAN communication support

I am currently in a process of selecting micro controller for my project. Basically i need TTCAN support and i have STM32F746G Disco board with me. Now as per the ST reference manual i see that this is supported. Now my questions are...Is there any ...