uSDCard on STM32F746G-DISCO
I am working with STM32CubeMX 4.26.1 and uVision V5.25.2.0 on card STM32F746G-DISCO
First, I use the program given in example “en.stm32cubef7\STM32Cube_FW_F7_V1.12.0\Projects\STM32746G-Discovery\Applications\FatFs\FatFs_uSD�?
This example works but I can’t integrate it in my code.
There is no ‘*.ioc’ file attached (from STM32CubeMX)
So I can’t include this file in my code.
Second, I try with internet tutorial named “12 SD card Programming on STM32F7 Discovery Board using Keil uVision�? , “13 SD card …�? , “14 SD card …�?
Address : https://www.youtube.com/watch?v=kRhF44v2ezM
But, at the begin, 2 declarations are invalid because already declared in another file.
Already declared in “fatfs.c�?
char SDPath[4]; /* SD logical drive path */
FATFS SDFatFS; /* File system object for SD logical drive */
When I comment on these lines, the program can run but it does not realize the f_mount.
I have been working on this program for a week and I am at the end of my abilities.
Does anyone have an idea, a * .ioc file and the * .uvprojx project or something to help me?
Sorry for my English,