STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Long period timer interrupt

I am using a STM32F401RE board and I want a timer interrupt to trigger every minute. I have tried it using timers. Here is my code: main.c  TIM_HandleTypeDef htim10;  int main(void)  {  HAL_Init();     SystemClock_Config();    // Some other code  MX_...

pbdiazam by Associate II
  • 2914 Views
  • 3 replies
  • 0 kudos

PROBLEM WITH PERIPHERAL POST-INCREMENT USING DMA - STM32F100VC

Hi,I am using DMA to transfer the conversion of two injected channels of the ADC module (registers ADC1_JDR1 & ADC1_JDR2) to a buffer in ram. The conversion is started by software (JSWSTART).Since the transfer is for two consecutive records, I have s...

FTrnp by Associate
  • 1882 Views
  • 3 replies
  • 0 kudos

Measuring capacitance STM32F103 using HAL_Library

Hi, i'm trying to measure capacitance using a single GPIO pin ( found an article online a guy used this method to calculate the diode reverse current so i'm guessing its possible to measure capacity aswell). Firstly i use the pin as output and charge...

RSabl by Associate II
  • 4273 Views
  • 4 replies
  • 0 kudos

How to program STM32F407 using STM32Cube programmer?

Can't program STM32F407 because address is not supported for SWD/JTAG port.Hello, I am trying to begin developing drivers for the STM32F407VG. I am using Atollic TrueSTUDIO as IDE. For loading the programs to the board I am using Exteral Tools config...

0690X000006Df9EQAS.png
MAhme by Associate
  • 1325 Views
  • 1 replies
  • 0 kudos

Changing the pin configuration at run-time

Posted on July 17, 2017 at 09:17 Hi All, I would like to read a resistive touch screen with a STM32F407 micro butwithout a driver chip. For that I should change the pin functionality at run-time. First I set the configurations like below: ...

flash and CAN conflict?

Hello everybodyI was trying to store some data into flash and every time the erase page failed, the write completed if the memory was empty.I then found out that the erase is working until I send something over the CAN ( receive seems to not trip it)...

MA2 by Associate
  • 1422 Views
  • 1 replies
  • 0 kudos

Problem with USART communication between 2 processors

I have two STM32H743 processors which are connected by USART ports. We have to transmit data between these 2 µPs and have no other ports left (SPI or so) which could be used instead.I initialized the 2 USARTs using STM32CubeMX with the identical sett...

GS1 by Senior III
  • 2396 Views
  • 4 replies
  • 0 kudos

Programming STM32F730s from other STM32F730s

I need to program a large array of STM32F730s from a single master STM32F730. ST seems to have lots of applications notes on using bootloaders to pull code into these devices, and also on using STM-LInk to push code in. But what I need to do is pus...

MikeDB by Lead
  • 2848 Views
  • 10 replies
  • 0 kudos

SPI 1 line simplex rxonly

Hello, How to read data from slave in 1 line rxonly. I have this set up STM3f446re board as master and arduino uno as slaveMaster and slave are connected through only 2 lines. MISO and NSS. Master will be in rxonly mode and slave sends data to master...

n.serina by Associate III
  • 1344 Views
  • 3 replies
  • 0 kudos