STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Run-time UART Buadrate change

I am working on STM32L462CE MCU and my requirement is to change the baudrate of UART at run-time. So, how I do that?. Can you please give me the solution for this. First set to 9600bps, after 921600 and at last 115200.

AP_040 by Senior
  • 2371 Views
  • 7 replies
  • 0 kudos

How do I configure ETM tracing on an stm32?

Hello, I am trying to use a segger jtrace pro debugger with an stm32303E-EVAL board through the ETM trace connector, however I am not seeing a signal on any of the trace pins including the trace clock when running my program. I've ensured I have cont...

AOlve by Associate
  • 1438 Views
  • 2 replies
  • 0 kudos

What criteria (requirements) are used to determine the HSE clock has failed (sets the CSSF interrupt in the RCC_CIR register) on a stm32f103x processor?

Documentation simple says the HSE clock failed. What does "fail" define. Does "fail" imply that there are no clock oscillations applied to the HSE pins? Or a frequency below some value that will set the CSSF flag in the RCC_CIR register. What would b...

bgabl by Associate
  • 557 Views
  • 0 replies
  • 0 kudos

NUCLEO F722ZE CubeMX CDC USB not enumerating ? Try this ...

Hi, I just want to give a short workaround for an issue i had with the NUCLEO F722ZE board. The CUBE-MX project (NUCLEO F722ZE selected - no custom build) does not work out of the box for CDC devices. In order to fix it i changed the default CUBE-MX ...

ThiZi by Associate
  • 1136 Views
  • 2 replies
  • 0 kudos

how to blink 2 LEDs with a Timer?

Hello everybody,I wanted to turn 2 LEDs with Timer on / off. The period is 4s and the first LED should be on for 2s and off for 2s. and then the 2nd LED should do the same but not at the same time. But unfortunately I can not do that with a timer and...

Samuel1 by Associate III
  • 2839 Views
  • 3 replies
  • 0 kudos

STM32F030R8 pinout questions

The Rev 4 data sheet for the STM32F030R8 lists the pins for SPI1 on both pins 20-23 and 50,55-77. I2C1 on 58-59 and 61-62, andUART1 on 42-43 and 58-59Which is correct, or are they selectable via registers?

LPoly by Associate
  • 1116 Views
  • 1 replies
  • 0 kudos

STM32F407 Timer->DMA->GPIO

HelloI'm trying to use DMA to directly write on GPIO port, and I've attached the code snippet I'm using to do so.But, I'm getting this exception which is stopping the DMA and fails writing data.Any thoughts?Regards.GPIO Init:__HAL_RCC_GPIOD_CLK_ENABL...