cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to configure the IWDG timer to 30 minutes?

Khoo.B
Associate III

I have an IoT hardware (using STM32L152) that carry out some tasks and go to STOP mode for 30 minutes. Then, it will wake up and repeat the same process again.

Now, I would like to add the watchdog timer to ensure everything works fine. My question is - can we set the countdown timer to 30 minutes? I have seen on other discussion that it is not possible to configure the watchdog timer to such a long period.

Any suggestions? Thank you very much!

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5

I think you'll find the counter and prescaler are too small.

Think you have to use RTC Alarm(s)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Jeroen3
Senior

@Community member​ is right. Maximum 28 seconds.

Khoo.B
Associate III

Ok, thanks for the suggestion. Would it be possible to turn it off?

I have seen in other discussions that an alternative work around is to wake up from the STOP mode every <28 seconds to reset the counter. Would this have a significant impact to the power consumption?

AvaTar
Lead

An once activated watchdog timer cannot be turned off.

For an application with 30 minutes sleep times, I would not consider a watchdog.

Khoo.B
Associate III

What would you recommend in this case? An external watch dog?