cancel
Showing results for 
Search instead for 
Did you mean: 

Hi Is it possible to connect the internal hard drive to STM32 ? How?

gamer
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Jeroen3
Senior

It is theoretically possible to connect a SATA hard disk using an USB to SATA bridge IC.

The STM32 must work in USB host mode, and support the device class of the hard disk.

If it is any practical, I'm not sure. It will be pretty slow, and you can't use GPT or NTFS unless you find firmware for that.

IDE ones would be easier.

On the platform people typically use eMMC or microSD cards. You could add 400GB​ to a project that way.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

Internal to what? Try to describe your idea in one-two sentences.

JW