STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I change the DMA stream?

Hello everybodyI am a student trying out some things with the evaluation board STM32F769I-EVAL.First, I think it is important to say that I have nearly no experience with STM controllers.So, let's look at my problem. The main aspects I am looking at,...

Resa111 by Associate
  • 958 Views
  • 1 replies
  • 0 kudos

Use rising/failling edge to start PWM

Hello, I work on STM32F407.I want to start the PWM 1 on the rising edge of the main PWM and start the PWM 2 on the failling edge of the main PWM. But I don't know how I can detect the rising/failling edge...Can you help me please ? Thanks a lot.

FightKol by Associate II
  • 1760 Views
  • 4 replies
  • 0 kudos

HAL_CAN_AddTxMessage() issue

Posted on June 13, 2018 at 21:06 Hi, I am using Nucleo-144 connecting CAN RX/TX PD0/PD1 to external CAN transceiver, PEAK. The function is pretty straight forward. Prepare data then call HAL_CAN_AddTxMessage() to transmit. CAN_TxHeaderTypeDe...

Dick Lin by Senior
  • 13277 Views
  • 14 replies
  • 0 kudos

STM32F446xx - measuring system clock on MC01

Hello everyone,I have a development board with the MCU specified in the title. I have used Keil to create a project and flash my board. According to what I understood from the documentation I read and by looking at the startup code:MCU is by default ...

PPopo by Senior
  • 4278 Views
  • 8 replies
  • 0 kudos

Resolved! Unable to set PLL as main clock derived from the HSI

Hi All,I am working with the STM32F302R8. I want to set the system clock as the PLL through derived from the HSI. I want a clock of 64MHz which I should have set through the appropriate registers.I think I have set all I need however, after the RCC c...

glenn0010 by Associate III
  • 3387 Views
  • 3 replies
  • 0 kudos

STM32F427 suddenly in Read Protected Secure Mode

Developing code / debugging 2 days ago and all was well.This morning I attempted to flash the mcu (using ST-Link / V2) and it reported back that the Processor failed to halt.Switched to my J-Link and it reported that the MCU was in an Active Read Pro...

Joe.H by Senior
  • 1059 Views
  • 3 replies
  • 0 kudos

Flash write/Read program does not work with debugger

I am working with G071 neucleo board. I am trying to debug a program that writes and reads for EEPROM emulation. However, it does not work as expected in dubug mode. The example program provided by ST for Flash runs well in run mode ( Without debugge...

NGT by Associate
  • 860 Views
  • 1 replies
  • 0 kudos

Resolved! External SRAM issue

Hello,I hope someone can help with this riddle.We just started working with our custom board, based on stm32h743 (untill now we worked with eval stm32h743-eval board).The internal memories, GPIOs and other interfaces works OK, but we have the followi...

ranran by Senior II
  • 1462 Views
  • 4 replies
  • 0 kudos

Sector Erasing in STM32--chip crashes on 256kB erase

I am working on erasing sectors sequentially in my MCU, from Sector 2 through Sector 7 (the size of flash where my firmware will live). I have found that sequential sector erases will occasionally fail, and any attempt to erase a sector of size 256k...

rsoc by Associate III
  • 2067 Views
  • 4 replies
  • 0 kudos