STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

production ready STM32 boards

Hi,Does anyone know if there are any companies out there that sell production ready stm32 hardware boards. I appreciated there would be a lot of variations regarding io etc.. but i just wondered if it was a "thing" or if the only board are typically ...

Resolved! STM32L431 can't enter STOP2 mode

I'm trying to enter STOP2 mode to save energy but the MCU get stuck in the function HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI). I have cleared all EXTI pending flags and RTC flags, and disable all five wake up pins. The MCU is supposed to wake up vi...

TClar.8 by Associate II
  • 7398 Views
  • 11 replies
  • 0 kudos

Resolved! STM32 General Purpose Timer Update Event and glitch problem

I use STM32F102 and TIM2 timer in PWM1 mode to generate defined frequency and duty cyclesquare wave. I have some questions and I hope can get some help from experienced colleagues.1. I update the ARR/CCR1 register in an interrput which is defined by ...

NCTUser by Associate III
  • 6273 Views
  • 5 replies
  • 0 kudos

I am working on STM32H743 micro operating as a slave I2C device. I am able to write to the slave device by a master I2C device but I can't seem to read.

I have done some investigation and arrived that the problem is with the "DIR" bit in the Interrupt Status register not firing to indicate whether to do a Read.uint32_t isr_trace[64]; int isr_count = 0;   void I2C2_EV_IRQHandler(void) { isr_trace[...

onio by Senior
  • 1986 Views
  • 5 replies
  • 0 kudos

[How to] From Mechanical to Capacitive controls Guide (Buttons with sharp edges and 2mm clearance, 2 layer pcb with cover glass (50x70mm))

Even though most of you may be relatively familiar with the various types of mechanical controls, the same does not necessarily apply for capacitive ones. So, let’s start off by defining the most basic elements of capacitive sensing.Capacitive button...

PAram by Associate II
  • 1650 Views
  • 0 replies
  • 1 kudos

F4 DMA2 errata - how to handle that

Hello!We have choosen the STM32F407/427 for our product, a couple of years ago.It fits with the speed, and also with the possibility to use DMA for mutliple peripherals.Now, as we have found out the hard way, the DMA2 fails while handling ADCs and SD...

a.n by Associate II
  • 3920 Views
  • 7 replies
  • 0 kudos

STM32F051C8 ADC Accuracy Problem

Hello,I've been using STM32F051C8 on some of my projects and I recently realised that, my ADC is not converting accurately. I connected my Vdda to Vdd, that is 3,3VDC and tried conversation routine below.Here is the initialisation: Single Channel con...

RDermenci by Associate II
  • 4297 Views
  • 9 replies
  • 0 kudos