Associate
December 14, 2018
Question
PWM on TIM1 CH1 of NUCLEO--F303RE does not start
- December 14, 2018
- 5 replies
- 1445 views
Hello,
I dont't know why in my projetc the PWM daoes not start.
I would generate a PWM with Duty =50% and Period =10msec. I use a NUCLEO--F303RE.
I started with CubeMX to generate the project configuring IO (blinking the green LED) and the PWM on TIM1 CH1 setting the output on PA7.
I see the LED blinking correctly but PWM not working. I see PA7 fixed at 3.3V.
Can you tell me where is my error please? I attach the project Truestudio end CubeMx
Thank you in advance
Marco