STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDRAM Extended Mode Register Write

I am using an STM32F769NI with a MT48H16M32LFB5-6 SDRAM chip, everything works fine. we are looking to set the drive strength to 1/4, 1/2 and full to evaluate the effect on EMC testing. From what I read in the programming manual, it states to perform...

0690X000008id91QAA.png 0690X000008id96QAA.png
gvigelet by Associate II
  • 632 Views
  • 0 replies
  • 0 kudos

How to properly configure the CAN2 RX Interrupt on STM32 ?

Hello,My RX0 Interrupt is not called and I don't understand why. If someone can help me, because I already tried lot of things.The problem is I never go in my "CAN2_RX0_IRQHandler()".I properly configured my CAN timings because the received frames ar...

ALuca by Associate II
  • 976 Views
  • 0 replies
  • 0 kudos

STM32 I2C multi-device connection

Hello to everyone, I am a newbie on STM MCUs. I need to communicate 6 slaves and 1 master device. But I could not figure out. The master device has been selected Arduino mega due to some specifications. Slaves are responsible to drive motors, Arduino...

Sensortile standby high consumption

I am working on a project using the sensortile. When the MCU is not in use, it enters a standby mode. I measured a current of 4.5 mA in standby mode. What could be the cause of such a high consumption in standby mode?

RMous by Associate
  • 1485 Views
  • 3 replies
  • 0 kudos

Losses the bytes of data in LPUART IRQ HANDLER?

I have configured LPUART with 9600 baud rate and enable receiver interrupt with MCU 65Khz low power mode and my uart handler likevoid LPUART1_IRQHandler(void){ uint32_t isrflags  = READ_REG(hlpuart1.Instance->ISR); uint32_t cr1its   = READ_REG(hlpuar...

Uart timeout?

Hi,I am using LPUART for sending data to the GSM. I wrote own uart transmit driver without timeout, like void LPUART1_Send_Data(uint8_t *string){ while(*string) { if((LPUART1->ISR & USART_ISR_TC)==USART_ISR_TC) { LPUART1->TDR=*string; ...

HAL_SRAM_Read_DMA() assumes 8-bits word ?

Hello,When using SRAM without DMA I find several group of APIs for read/write, depending on bus width:HAL_SRAM_Write_8b HAL_SRAM_Write_16b HAL_SRAM_Write_32band also read APIs of course.But for DMA there is only: HAL_SRAM_Read_DMAHAL_SRAM_Read_DMAIs ...

ranran by Senior II
  • 732 Views
  • 0 replies
  • 0 kudos