STM32F429ZIT6 doesn't start without debugging session
Hey Guys,
I have designed a custom board with the STM32F429ZIT6 which I programm with the STLink debugger together with TrueStudio. So far everything seems to work except that when I don't use a debugging session I have to manually make a reset on NRST pin or otherwise the processor will not start it's normal program execution. I have to do this every time power get's cycled.
I have one 4,7uF cap for overall buffering and then 10nF and 100nF at each Vdd and an extra ferrite bead for the Vdda pin but with 1µF and 10nF as a decooupling. I did not implemnt a 100nF cap from NRST to ground for short ESD burst but I doubt that this is the cause for the problem since after the manual reset everything works fine.
Do I maybe need a reliable power cycling with an external power supervisor chip doing the manual reset, or did I do something comepletely wrong?
My controller runs with 3,3V.
best regards
Benjamin