STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L432KC - Bootloading from RFID I2C Memory?

Hi all,I develop rough environment IoT sensors that are completely potted in polymer epoxies. I use a STM32L432KC MCU inside to drive different sensors and RF radios. My sensors also integrate I2C RFID memories and magnetic switches in order to inter...

XBLYNKZ by Associate II
  • 2228 Views
  • 5 replies
  • 0 kudos

Resolved! stm32f411 spi4 low clock speed

Hello!I have problem with spi4 clock speed. I want to drive a lcd tft display but spi clock is max 500Khz, baudrate prescaler set to SPI_BAUDRATEPRESCALER_2. Is very weird. Initial setup was made with CubeMX to 48Mbit/s. APB2 clock is set to 96Mhz. I...

mcufan by Associate III
  • 10650 Views
  • 18 replies
  • 0 kudos

FMC Issue with Allignment

I am trying to read/ write data into FMC SDRAM (16 bit) in Bank 1. While writing the data hard fault occurred. What is the reason for that hard fault, is there any problem with data alignment, If yes what is the solution for it ?

PBU by Associate III
  • 937 Views
  • 1 replies
  • 0 kudos

Interruption each 10 seconds with RTC

Hi guys,I'm using STM32LO and i try to implement a code who aquire data of a sensor every 10 second in a fix day in a week. The rest of the time, the ship is sleeping.I'm trying to do that interruption with RTC and i configure the RTC and program my ...

0690X000009YvlDQAS.png 0690X000009YvlIQAS.png 0690X000009YvlNQAS.png
mibou23 by Associate II
  • 2652 Views
  • 2 replies
  • 0 kudos

STM32L451VC: Problems with ADC.

Hello, I'm working with a PCB based on STM32L451VC MCU and I have different problems with the ADC. I'm trying to measure an input channel using the HALs provided by the STM32CubeMX but I can't achieve it. The main problem is that the bit ADRDY from A...

Luis Ber by Associate II
  • 761 Views
  • 0 replies
  • 0 kudos