STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why SDADC could't not start

Hi everyone,I designed my custom board with stm32f373c8. SDADC runs properly when voltage reference is setted with Vref or VDDA. But when voltage reference is setted with internal 1.8 volt or internal 1.2 , sdadc could't start. It waited while loop t...

Sy??n by Associate
  • 882 Views
  • 0 replies
  • 0 kudos

STM32F042 CAN POLLING WORKS - INTERRUPTS NOT HAPPENING

I have coded it both ways, so the hardware and software works except when switching to interrupt-driven receive. No interrupts happen, though I have checked and rechecked. The global NVIC can interrupt setting is there, and the enable. The CAN priori...

GBats by Associate
  • 719 Views
  • 0 replies
  • 0 kudos

CAN Bit Stuff Error during CAN2 pins initialization

Hi,I am using STM32F103RFT6 64 pin package mcu. i am seeing can bit stuff error during CAN2 TX pin ( PB9) initialization. when mcu is in reset state this pin is in high state, the moment CANTX pin gets configure to Alternate function pushpul, Low s...

YKuma by Associate
  • 951 Views
  • 0 replies
  • 0 kudos

SDIO multiple block write

Hello,I'm working with SDIO to write data to a sd card and I'm using DMA. The basic process of my project is :1.Get 512 bytes data from an external ADC 2.Write it into a SD card3.RepeatI want to use the multiple block write mode, but everytime just s...

DSun by Associate
  • 1740 Views
  • 2 replies
  • 0 kudos

STM32F051 touch library bug

Hi,I Have two problem.first : using STM32F051R8Txcant use IO_TOUCHKEY2 at all !, have to assign IO2 to unused PIN and define new IO_TOUCHKEY.(if you need 3 touch you have to set 4 touch in CUBEMX case IO_TOUCHKEY2 doest respond!)second: why STM32F051...

HNaja.5 by Associate
  • 608 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F072C8 Total Flash Memory?

Hi guys,The STM32F072C8 microprocessor has a total of 31 flash pages. Each page is 2 kb in size. Thus, the processor has 64 (2x32) kb flash memory. The interesting thing is that I can read / write on page 63. How is that possible?Thanks.

Hi world! by Associate III
  • 3564 Views
  • 9 replies
  • 0 kudos