STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Read and write Bluetooth communication byte format

Hi Community, ​I'm studying about the android program and stm32f407vet based controller.​The question I asked before is almost clear by using DMA USART.I'm Transmit and Receive like under code.code(IN STM32)uint8_t rxBuffer;int SIZE_OF_RX_TX = 1;if (...

BSang by Associate III
  • 2665 Views
  • 3 replies
  • 0 kudos

Resolved! TIM6 undefined interrupt reason on STM32H753I eval board

Dear experts,I'm struggling with a strange TIM6 interrupt issue on STM32H753I.Playing with one of Cube example projects with FreeRTOS, where TIM6 is used as HAL timer.The original IRQ handler is very simple (and the demo works fine) :void TIM6_DAC_IR...

Pavel A. by Super User
  • 2323 Views
  • 3 replies
  • 1 kudos

Micro Trace Buffer (MTB) in STM32L0 devices?

Figure 1 in STM32L0 Series Cortex®-M0+ programming manual (PM0223/DocID025763 Rev 3) shows a "Micro Trace Buffer (MTB)" on the top right. I could not find further information on that, neither in the reference manual RM0377 nor in the data sheet of ST...

seren by Associate III
  • 2676 Views
  • 3 replies
  • 0 kudos

Challenges in having 8 SPI slaves on single SPI bus?

Hello all,In my application I am supposed to use 8 similar SPI slaves on single SPI bus with master as (STM32L452RCT6) with different chip select lines for each slave. Also, please let me know if it is necessary to configure the CS lines on same Regi...

YVerm by Associate II
  • 2902 Views
  • 5 replies
  • 0 kudos

Different return paths for STPM33 ICs?

Hello all,Since i was not able to find thread for Power Monitoring ICs, hence, posting my question here.I am using STPM33 PM IC for my application and i have below queries:-As i can see in the datasheet in the application schematic column, two ground...

0690X00000AAFwgQAH.png
YVerm by Associate II
  • 3058 Views
  • 2 replies
  • 0 kudos