cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f030c8 Flash write protection error

l239955_st
Associate II
Posted on March 16, 2015 at 10:58

Hi,

I'm wrtiting a bootloader for updating an embedded product. Bootloader sequence seems correct now and I want to protect from writing the bootloader flash addresses. Using the snippets of code from St this is my code:

void Check_Write_Protection( void )
{
// unlock the Flash Program Erase Controller (FPEC)
FLASH_ClearFlag(FLASH_FLAG_EOP | FLASH_FLAG_WRPERR | FLASH_FLAG_PGERR | FLASH_FLAG_BSY);
ProtectedPages = FLASH_OB_GetWRP();
// pages are not write protected 
if(ProtectedPages == 0xFFFFFFFF)
{ 
FLASH_OB_Unlock();
res = FLASH_OB_EnableWRP(OB_WRP_Pages0to3|OB_WRP_Pages4to7);
FLASH_OB_Lock();
NVIC_SystemReset();
}
}

the problem is when I call the

FLASH_OB_EnableWRP,

the flag for write protectione seems unlocked but i have a FLASH_PROGRAM_ERROR when I call :

if(WRP0_Data != 0xFF)
{
OB->WRP0 = WRP0_Data;
/* Wait for last operation to be completed */
status = FLASH_WaitForLastOperation(FLASH_ER_PRG_TIMEOUT);
}

OB->WRP0 = WRP0_Data

set PGERR = 1 in SR register and so memory is non protected.

Any suggestion? What am I missing?? Thanks a lot
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Posted on March 16, 2015 at 12:23

What am I missing??

Probably a FLASH_Unlock()? or to erase the options.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
l239955_st
Associate II
Posted on March 16, 2015 at 12:28

Hi Clive,

first of all thanks for your response.

Well I've tried the flash_unlock() and flash_lock(), but it seems the same. What do you mean with the Erase Option? I have to copy the value of option bytes then erase them ?

Thanks...

Posted on March 16, 2015 at 12:37

Flash memory needs to be erased before it is re-written.

FLASH_OB_Erase() would be needed if you change the option(s). And yes you'd probably need to evaluate the current state and save it prior to the erase so you could restore the other option settings.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
l239955_st
Associate II
Posted on March 16, 2015 at 12:49 Tried this...not working...sigh HSI is enabled and I'm using st link 2 with SWD... Do you have any other idea Clive? A strange thing...when I read option bytes I get 0xFF but in the debugger register I don't see 0xFF

void Check_Write_Protection( void )
{
// unlock the Flash Program Erase Controller (FPEC)
FLASH_ClearFlag(FLASH_FLAG_EOP | FLASH_FLAG_WRPERR | FLASH_FLAG_PGERR | FLASH_FLAG_BSY);
ProtectedPages = FLASH_OB_GetWRP();
// pages are not write protected 
if(ProtectedPages == 0xFFFFFFFF)
{ 
FLASH_Unlock();
OPBByteCpy = FLASH_OB_GetUser();
FLASH_OB_Unlock();
FLASH_OB_Erase();
res = FLASH_OB_EnableWRP(OB_WRP_Pages0to3);
res = FLASH_OB_EnableWRP(OB_WRP_Pages4to7);
FLASH_OB_WriteUser(OPBByteCpy);
//FLASH_OB_Launch();
FLASH_OB_Lock();
NVIC_SystemReset();
}

l239955_st
Associate II
Posted on March 16, 2015 at 15:18

St Link utility works fine...:(

I don't really know where's the problem....

Posted on March 16, 2015 at 17:00

Don't rely on the debugger, it's invasive, instrument your code, and understand the error returns, and status of the flash controller, in the cases where it is failing.

Have the code stop earlier if it gets an error.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I'm also trying to implement something similar.

I don't understand what you are trying to do - by saving the state to OPBByteCopy and then writing it back again - you are not effecting any change...unless somehow the function FLASH_OB_EnableWRP changes the value of OPBByteCopy

Were you able to get this to work?

Thanks,

Mechi