User Activity

@Winfred LU​ Hello i have been using bluenrg-2 module for quite some time and i have noticed that after working well for the 2-4 days continuously sometimes the module does not show up in scan request i.e. it does not advertises. I'm sure the while t...
What is ST system bootloader address. I want to jump the application code to system uart bootloader as the boot pin is not available as of now.Thanks@Winfred LU​  @Eleon BORLINI​ 
@Eleon BORLINI​ Greetings of the Day Currently I am using LSM6DSM as my IMU. Now in this sensor I need to write my own function to obtain the quaternions and then based on that obtain the roll, pitch and yaw of the system. The question that I have is...
Hello, I'm trying to use two identical stm32f4 boards to synchronize tick of one with respect to other.I'm using can to using can protocol for communication in Interrupt mode.So the Master is supposed to be always running and the slave when powers up...
Hello, We are going to start working on LSM6DSM sensor. We have read that it a vibration monitoring functionality. We just wanted to know that can a vibration of certain threshold generate an interrupt on one of the two interrupt lines. There is not ...