STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The question pertains to maximum rise time specification for STM32L151CC OSC32_IN when Low-speed external user clock is generated from an external source.

The question pertains to maximum rise time specification for STM32L151CC OSC32_IN when Low-speed external user clock is generated from an external source. This specification, according to the datasheet, is 10 nano seconds. This seems unreasonably fas...

faizal by Associate
  • 757 Views
  • 0 replies
  • 0 kudos

STM32H753AI Recommended Footprint

Hello,In the STM32H753AI datasheet, there are footprint guidelines for all the packages, except for the UFBGA169 (see attached image).Has anyone built a board with this package? Where did you find any info on this type of package?Is there a database ...

Yan Rosh by Associate II
  • 2919 Views
  • 3 replies
  • 0 kudos

I2C Library for PCA9685 won't work

I'm creating an I2C library for PCA8596 to control servos using STM32F4 Discovery as master. I already checked the PCA using arduino, and it worked. It also compiled well and can be uploaded.The problem is the SCL and SDA from the stm didn't generate...

Uwii by Associate
  • 1468 Views
  • 0 replies
  • 0 kudos

AN4861 for 'H7

ST,Please update AN4861 for 'H7Please link to AN4861 from the 'H7 product folder webpagesPlease fix links to AN4861 on forum - those given by Amel and Imen are usually broken, you can find them by searching for DM00287603Thanks,JW

Regarding Auto grade Controller in stm32h7 series

Hello everyone, I want to work on STM32 series of controller which supports 480MHZ or above clock rate and Auto grade temperature range(I.e Grade0: -40degc to 150degc (or) Grade1:-40degc to 125degc).We found STM32H7 series which supports our applica...

BSRIL by Associate
  • 1202 Views
  • 1 replies
  • 0 kudos

Documentation issue RM0385 (F7)

https://www.st.com/content/ccc/resource/technical/document/reference_manual/c5/cf/ef/52/c0/f1/4b/fa/DM00124865.pdf/files/DM00124865.pdf/jcr:content/translations/en.DM00124865.pdfReferences to OPT instead of OTP

0690X00000ARAH8QAP.jpg

Resolved! STM32F769 Discovery kit demo firmware

Hi,I ran several test and example projects on the STM32F769 Discovery platform. I would like to reload the original demo firmware. According to the documentation, it should be available from the www.st.com/stm32f7-discovery webpage but I cannot find ...

TPier by Associate III
  • 6570 Views
  • 11 replies
  • 0 kudos