STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G070CB: What are Flash Zones A and B?

The HAL Manual for the STM32G070xx mentions OB_WRPAREA_ZONE_A and OB_WRPAREA_ZONE_B. The Reference Manual mentions Zone A and Zone B. But there is no mention of the difference between the two or when to use one vs the other. There are 64 pages of Fla...

DBroo.1 by Associate III
  • 1199 Views
  • 1 replies
  • 0 kudos

STM32F051K8, I2C and UART Communication Issue

Hi,I am trying to receive voltage from an external ADC, MCP3421 using I2C. These values are then transmitted over USART to be viewed by the user ranging from (-2.048 to 2.048). The MCU I am using is STM32F051K8.The problem that I am facing is that th...

Shirish by Associate II
  • 1555 Views
  • 3 replies
  • 0 kudos

Has a problem when using STM32F405 spi + dma as a slave

Use STM32F405's SPI + DMA as a slave, circular mode, DMA 16bytes interrupt, but every time send 16bytes to master, the first byte is always the byte that last frame's last byte , it looks like spi tx register is not clear, always contain the last by...

CJi by Associate II
  • 4712 Views
  • 11 replies
  • 0 kudos

STM32F7 Timer Event Generation Register Wrong address?

Hello I'm using a STM32F769 discovery board. I was trying to use timer2channel2 to trigger the ADC conversion. I am setting registers manually and wanted to turn on event generation on channel 2 match. TIM2->EGR |= TIM_EGR_CC2G_Msk;However when I ran...

Resolved! I'm trying to blink one led but two led blinks

Hi,i'm trying to blink only one led. I have a problem with one of four leds. Because as you in my code, i'm trying to blink only 'green led'. But 'blue led' blinks also. #include "stm32f4xx.h" // Device header #include "stm32f4xx_hal...

STM32 trying to get uasart to transmit

Hello, I wanted to upgrade my simple blinky program with the usart 2, so that it sends a simple 'B' over the serial port to my PC. I am using a Nucleo-F334R8. In the datasheet it says usart2 is connected with the USB port.Here is my code, that is not...

Facing issue while flashing code in STM32H745 Disco board?

Hi , I am trying to flash my code of GPIO toggle into the STM32H745 Disco board,but it is giving the error .While building the project I have seen an error "GPIO_CM4\GPIO_CM4.sct(7): error: L6235E: More than one section matches selector - cannot all...

psiva.13 by Associate II
  • 1050 Views
  • 0 replies
  • 0 kudos