cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 RevV Flash Programming and AN5312, where is the difference?

Uwe Bonnes
Chief

RM0433 Rev 5 writes:

The recommended single write sequence in bank 1/2 is the following:

1. Unlock the FLASH_CR1/2 register, as described in Section 3.5.1: FLASH configuration

   protection (only if register is not already unlocked).

2. Enable write operations by setting the PG1/2 bit in the FLASH_CR1/2 register.

3. Check the protection of the targeted memory area.

4. Write one Flash-word corresponding to 32-byte data starting at a 32-byte aligned

   address.

5. Check that QW1 (respectively QW2) has been raised and wait until it is reset to 0.

An5312 Rev 1 writes:

The recommended write sequence is updated as follows:

1. unlock the FLASH_CR1/2 register (only if register is not already unlocked)

2. enable write operations by setting the PG1/2 bits in the FLASH_CR1/2 registers

3. check the protection of the targeted memory areas

4. write one Flash memory word (corresponding to 32-byte) data starting at a 32-byte

   aligned address

5. check that QW1/QW2 (respectively for FLASH_CR1/2) has been set high and wait until

   it is reset to 0.

I have read multiple times and beside wording, where is the difference?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello,

In fact, the change was anticipated and implemented in the RM.

Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen