STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051R8 TIM14 does not work

Hi,I'm practicing with the timers of my STM32F0-Disco.Quite simply, I'm trying to use TIM6 or TIM14 as a simple time base. In order to verify its correct functioning I have put a GPIO call to toggle a LED whenever the interrupt handling function is c...

MMazz.11 by Associate II
  • 2424 Views
  • 5 replies
  • 0 kudos

Double Speed Systick STM32F042

I configured a Project with STM32CubeMX 5.3 for STM32F042. Using Nucleo-Board witch Jumpering for MCO from STLink..The 1ms Timer works fine when using HAL for RCC, but it goes double Speed when changing RCC to LL. I have to limit Codesize for a Boot...

STM32F302 ADC Pin Negative Injection Current

Recently started working on an STM32F302, and am having a really odd issue with the ADC. It seems that there is current coming out of the ADC pin. We have a 10k resistor with an anti-aliasing filter feeding the channel, and we see current flowing out...

vielster by Associate II
  • 3674 Views
  • 7 replies
  • 0 kudos

I want to make Comparator's output inversely.

Hello, I am using STM32 L031K6 & its low power Comparator, which is running in stop mode.​What I want to Comparator is:when pin PA3's input voltage is bigger than reference Voltage, then Comparator give interrupt to the system. so after wake up from ...

DU2 by Associate II
  • 1098 Views
  • 1 replies
  • 0 kudos

Hi I'm new for STM32.I want to use Nucleo-f401re for my wireless design.The block diagram as per attached file.The EV2400 is interface module for battery management system BQ4050.I want to collect data from EV2400 via usb.

Then I want to call AT command to trigger LTE module EC25 and also transfer the data collected from EV2400 to EC25 by using Nucleo-f401re.Please advise the solution.

NAhma by Associate
  • 915 Views
  • 0 replies
  • 0 kudos

Resolved! What is the problem with this delay function?

Hi,i'm trying to create a delay function for microsecond delays. But it doesn't work. I couldn't understand where the problem is. Could you please let me know?(i'm using stmf030f4)edit: To understand where the problem is i'm trying to create a milise...

0690X00000AqQO3QAN.png 0690X00000AqQNyQAN.png

'F40x FSMC asynchronous WAIT clarification

RM0090 Rev.18 states in many places in the narrative that WAITPOL is used in the asynchronous modes (in the FSMC_BCRx bit fields tables for the various asynchronous modes, in WAIT management in asynchronous accesses subchapter, and elsewhere). Yet, t...

Can anyone document APBPrescTable ?

In the standard peripheral library, the array APBPrescTable is used to configure the clock prescaler values.Can anyone explain what these 16 values mean? How do they correspond with the prescalers described in the chip manual ("AHB Prescaler" etc.)?

RWhit by Associate
  • 1434 Views
  • 2 replies
  • 0 kudos