Beginner requesting an example of a timer interrupt every 20 us. Am using a Nucleo-F767ZI. Not sure if CubeMX is used for this as the interrupt is timer not external?
I am working to build a simple interrupt example of say 1 second with a 216 MHz STM32F767 however only one interrupt occurs. I have in my program read the relevant mcu registers to determine TIM3 clock is APB1 x 2 = 216 MHz. I have entered prescal...
I have with a simple 64 MHz Microchip displayed vertical bars of all the colors of red green and blue by use of an 8 bit resistor divider however clocking out the 640 pixels per line ended up being more like 4 horizontal pixels displayed in place of ...
Thanks for the information. DSI is on my radar and the HDMI adapter may be as well. I would like to have even a simple 1000 ms LED blink interrupt down as I am getting familiar with TrueStudio. I have tried mbed however am looking for more precise...