STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 can Acknowledgment Error

I am working with stm32f04c6 microprocessor.I've already sent data with canbus. now it does not work. status (tsr) code terro bit 1 is.there is no ackCAN error status register (CAN_ESR)LEC[2:0]=011; 011: Acknowledgment Error what should i do?////can ...

Communication between two FDCAN members and a third member transmit a CAN-FRAME which the two others should ignore. The thrid member ignores FDCAN-Messages

Hello everyone,I am using the NUCLEO-144 Board with STM32H743ZI.I would like to test the FDCAN with three members. Two of them use the FDCAN. The third one is an uC which accept FDCAN but cannot do anything the message of the two others. If I send me...

MSchn.14 by Associate
  • 885 Views
  • 0 replies
  • 0 kudos

Howto: Firmware Version Handling?

I'm new at stm32 processors and have a question about firmware handling. At the moment I'm using an uint value for the firmware version and it seems not to be the correct way. So what's the right way for doing this? Is there a register where I can sa...

STM32H743 UART read/write to/from PC and MCU

Hey there,I was wondering where I could find some resource materials for configuring UART to read and write to serial or if I could get a hand with it. Using CubeMX, I've enabled USART3, USB_OTG_FS, and and the USB CDC middleware, but still can't see...

Resolved! [STM32L431] Cannot monitor VBAT using ADC

I am trying to read VBAT value through channel ADC1_IN18.VBAT should be between 2.3 and 3.3V.VREF+ pin is connected to VDDA=1.8V.Values measured using ADC are linearly related to the real VBAT value, but I have not been able to get the exact value.Fo...

TClar.18 by Associate II
  • 4499 Views
  • 9 replies
  • 0 kudos